2015-03-24 12:05 PM
Hello, I am basing this post off of the STM32F0 firmware V1.5.
I am working on a CAN project where we recently migrated to a smaller package chip (we are now using the STM32F072RB). The firmware example for CAN networking uses the CAN bus on PORTD. However we are now using the CAN bus on PORTB (PB8, PB9). However i am unable to get the pin configuration to work at all. Below are the defines in main.h of the firmware example ported to portB.#define CANx CAN
#define CAN_CLK RCC_APB1Periph_CAN
#define CAN_RX_PIN GPIO_Pin_8
#define CAN_TX_PIN GPIO_Pin_9
#define CAN_GPIO_PORT GPIOB
#define CAN_GPIO_CLK RCC_AHBPeriph_GPIOB
#define CAN_AF_PORT GPIO_AF_1
#define CAN_RX_SOURCE GPIO_PinSource8
#define CAN_TX_SOURCE GPIO_PinSource9
Other than above the code is the same as the firmware example. I have gone through the much of the documentation and have been unable to find my error.
Thanks
#!stm32f0-!controlareanetwork
2015-03-24 1:10 PM
According to the
http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00090510.pdf
it's AF_4, not AF_1We’re moving the ST Community to a new platform to give you a better and more reliable community experience.