2016-09-10 3:37 AM
Hi every body.
i configure STM32CubeMX to write on SD card. im using stm32f7 discovery board. i set SDMMC on ''SD 4bit wide bus'' and enabled FatFS for SD card.my main function is :int main(void){ /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration----------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* Configure the system clock */ SystemClock_Config(); /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_SDMMC1_SD_Init(); MX_FATFS_Init(); /* USER CODE BEGIN 2 */ /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ if(f_mount(&SDDISKFatFs, (TCHAR const*)SD_Path, 0) != FR_OK) { /* FatFs Initialization Error */ Error_Handler(); }else { if(f_open(&MyFile, ''STM32.TXT'', FA_CREATE_ALWAYS | FA_WRITE) != FR_OK) { Error_Handler(); } else { res = f_write(&MyFile, wtext, sizeof(wtext), (void *)&byteswritten); if((byteswritten == 0) || (res != FR_OK)) { Error_Handler(); } } f_close(&MyFile); } while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */}after debug i found code hangs on f_open(&MyFile, ''STM32.TXT'', FA_CREATE_ALWAYS | FA_WRITE)is there any thing more to do , to make it work ??any help or suggestion would be appreciated.Thanks in advanceMA.2016-09-10 5:01 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.