2014-10-22 9:29 AM
Hello everybody!
Where can I download a previous version of the stm32cubemx? A newest version has generation bug, the generated c files not working. The initalization paramater sets in the structures but the init function does not called.2014-10-23 8:57 AM
Can you post the ioc of your failing project and where exactly the problem is in the generated files.
Thanks in advance, Regards Daniel2014-10-23 11:15 AM
Here is the project
The problem is in the i2.c rtc.c sdio.c crc.c files. If you see this fájl in the init funcitons there is no stm32hal function init call.2014-10-23 12:28 PM
I noticed the following problem in this new version:
15:37:20 **** Rebuild of configuration Debug for project board 168MHz Configuration ****
Info: Internal Builder is used for build
arm-atollic-eabi-gcc -c -mthumb -mfpu=fpv4-sp-d16 -std=gnu90 -DUSE_HAL_DRIVER -DSTM32F429xx -I..\..\..\..\Inc -I..\..\..\..\Drivers\STM32F4xx_HAL_Driver\Inc -I..\..\..\..\Drivers\CMSIS\Include -I..\..\..\..\Drivers\CMSIS\Device\ST\STM32F4xx\Include -Os -ffunction-sections -fdata-sections -g -Wall -o Drivers\STM32F4xx_HAL_Driver\stm32f4xx_hal_pwr.o ..\..\..\..\Drivers\STM32F4xx_HAL_Driver\Src\stm32f4xx_hal_pwr.c
C:\Users\monteiro\AppData\Local\Temp\ccrUEmDc.s: Assembler messages:
C:\Users\monteiro\AppData\Local\Temp\ccrUEmDc.s:315: Error: selected processor does not support Thumb mode `wfi'
C:\Users\monteiro\AppData\Local\Temp\ccrUEmDc.s:326: Error: selected processor does not support Thumb mode `sev'
C:\Users\monteiro\AppData\Local\Temp\ccrUEmDc.s:335: Error: selected processor does not support Thumb mode `wfe'
C:\Users\monteiro\AppData\Local\Temp\ccrUEmDc.s:343: Error: selected processor does not support Thumb mode `wfe'
C:\Users\monteiro\AppData\Local\Temp\ccrUEmDc.s:401: Error: selected processor does not support Thumb mode `wfi'
C:\Users\monteiro\AppData\Local\Temp\ccrUEmDc.s:412: Error: selected processor does not support Thumb mode `wfe'
C:\Users\monteiro\AppData\Local\Temp\ccrUEmDc.s:461: Error: selected processor does not support Thumb mode `wfi'
15:37:21 Build Finished (took 617ms) I created this project, only informing that the kit used.
The kit is STM32F429I-DISCOVERY I configured the application to generate one code for this kit. The program STM32CubeMX generated all the code and I did not modified anything! Im using the TrueSTUDIO Free to compile the project. Im attached one picture from TrueSTUDIO/Tools Settings and some configs: ASSEMBLER: COMMAND: arm-atollic-eabi-gcc -c All options: -mthumb -mcpu=cortex-m4 -mfpu=fpv4-sp-d16 -g -I..\..\..\..\Inc -Wa,--no-warn -x assembler-with-cpp C COMPILER: COMMAND: arm-atollic-eabi-gcc -c All options: -mthumb -mcpu=cortex-m4 -mfpu=fpv4-sp-d16 -std=gnu90 -DUSE_HAL_DRIVER -DSTM32F429xx -I..\..\..\..\Inc -I..\..\..\..\Drivers\STM32F4xx_HAL_Driver\Inc -I..\..\..\..\Drivers\CMSIS\Include -I..\..\..\..\Drivers\CMSIS\Device\ST\STM32F4xx\Include -Os -ffunction-sections -fdata-sections -g -Wall C LINKER: COMMAND: arm-atollic-eabi-gcc All options: -mthumb -mcpu=cortex-m4 -mfpu=fpv4-sp-d16 -T''..\STM32F429ZI_FLASH.ld'' -Wl,--start-group -lc -lm -Wl,--end-group -static -Wl,-cref,-u,Reset_Handler ''-Wl,-Map=${BuildArtifactFileBaseName}.map'' -Wl,--gc-sections -Wl,--defsym=malloc_getpagesize_P=0x1000 ________________ Attachments : TrueSTUDIO_free_01.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzRS&d=%2Fa%2F0X0000000bLz%2FeQhgSmWHS2hZxzuM7qodGRtI8DaH.qHAOz57AxS5W_A&asPdf=false2014-10-28 11:51 AM
Have you tested it?
2014-10-30 3:39 AM
Hi,
After checking with your project, it looks like a regression since 4.4 (seems to work with 4.3). To be rapidly confirmed by a deeper analysis, but as far as we can see, it is a bug. Instead of:arm-atollic-eabi-gcc -c -mthumb
-mcpu=cortex-m4
-mfloat-abi=softfp
-mfpu=fpv4-sp-d16 -std=gnu90
-D__weak=__attribute__((weak)) -D__packed=__attribute__((__packed__))
we have now:arm-atollic-eabi-gcc -c -mthumb -mfpu=fpv4-sp-d16 -std=gnu90 …
One colleague gave me a ''workaround'', acting on project settings in atollic: things to be changed in ‘Project … Build Setting’ (TargetSetting & ToolSetting), as shown on the attached screenshots. I'm gonna forward the message about the issue so that it can be fixed and integrated in a future release. Regards, Fred ________________ Attachments : atollic.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzRN&d=%2Fa%2F0X0000000bLx%2Fx4Loz48pSd54C.ESojxmB6rodjo0_eNxJDTA7fHYxMY&asPdf=false2014-10-30 8:07 AM
Thanks for the that. The problem is that I havent got 4.3 stm32cubemx installer and I havent found this. Can you send me a link with this?
2014-11-05 12:08 AM
Hello,
Please use the following workaround: in TrueStudio, open the ''Properties'' interface and verify the compilation settings, then press ''Apply''. Best Regards.2014-11-05 12:23 AM
Hello,
Can you help me about the generation bug?2014-11-05 7:59 PM
I am also having similar issues with Atollic True Studio Pro Eval. Auto-generated projects will not build. Mine also show up various processor does not support Thumb mode complaints.
I have tried the ST workaround without success. It still will not build. Can you give more information on your workaround please? I am brand new to ARM development though so perhaps I am doing something wrong. I also would appreciate a 4.3.x stable download link as I am trying to evaluate your tools and am unable to do so. ThanksWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.