2016-10-09 5:54 AM
hello,
I've been trying to set up some basic usb comunication with a usb mouse using my stm32f4 discvery. there are no usb examples for my board so I went in to look at other boards. I generated a project with cube inlcuding USB_OTG_FS in host only mode and four IO pins for LED's. I had a look in the files and it seemed like reading mouse buttons would be fairly trivial, but I can't make it work. if I run [code]devtype = USBH_HID_GetDeviceType(&hUsbHostFS);[/code] it detects the device correctly. [code]USBH_HID_MouseInit(&hUsbHostFS)[/code] returns USBH_OK but no matter what I try [code]mouse=USBH_HID_GetMouseInfo(&hUsbHostFS);[/code] is always NULL ''USBH_HID_MouseInit'' is never mentioned in the documentation(DM00105256.pdf) also, only the RTOS examples use them. Reading the standalone example, it would seem that to comunicate with a mouse would be as simple as runing GetDeviceType, and GetMouseInfo, but I can't get it to work. this is all the code I added, it's executed in the main while [code] if(Appli_state == APPLICATION_READY){ switch(state) { case 0: devtype = USBH_HID_GetDeviceType(&hUsbHostFS); if(devtype == HID_MOUSE){ HAL_GPIO_WritePin(GPIOD,GPIO_PIN_14,1); HAL_GPIO_WritePin(GPIOD,GPIO_PIN_12,0); state=1; } else if(devtype == HID_KEYBOARD){ HAL_GPIO_WritePin(GPIOD,GPIO_PIN_14,0); HAL_GPIO_WritePin(GPIOD,GPIO_PIN_12,1); state=2; } else{ HAL_GPIO_WritePin(GPIOD,GPIO_PIN_14,0); HAL_GPIO_WritePin(GPIOD,GPIO_PIN_12,0); } break; case 1: if(USBH_HID_MouseInit(&hUsbHostFS)==0){ HAL_GPIO_WritePin(GPIOD,GPIO_PIN_15,1); state=3; } else { HAL_GPIO_WritePin(GPIOD,GPIO_PIN_15,0); state=0; } break; case 3: mouse=USBH_HID_GetMouseInfo(&hUsbHostFS); if(mouse != NULL)HAL_GPIO_WritePin(GPIOD,GPIO_PIN_13,1); else HAL_GPIO_WritePin(GPIOD,GPIO_PIN_13,0); break; default: break; } } if(Appli_state != APPLICATION_READY) state=0; [/code]2016-10-11 6:53 AM
Hi nurd,
If you start from the example STM32Cube_FW_F4_V1.13.0\Projects\STM324xG_EVAL\Applications\USB_Host\HID_Standalone, then comment all board specific features, you should be able to run the example on your discovery board.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-09-21 5:27 PM
sorry, I have the same problem. I try to use stm32cube to configure usb host hid for communication with usb mouse but it's not work.
Please help me.
2017-11-14 9:03 AM
I run 4 examples in STM32F746G-DISCO, with RTOS, and standalone. The example that I run is the ones provided by st, without any modifications, and it didn't work.
2017-11-14 9:15 AM
I have also tested it on a custom board (stm32f401), and the same problem. It can comunicate with a microsoft keyboard, but when I plug a cheaper keyboard (leadership and other brands, chinese keyboards), it starts the keyboard, and disconects, I'm sure the keyboard works, and also STM32F746G-DISCO is supossed to work properly (works with microsoft keyboard). I'm compiling with sw4stm32.
2018-12-19 4:27 AM
I think you need two basic functions: MX_USB_HOST_Init() and MX_USB_HOST_Process();
[code]
int main(void)
{
[...]
MX_USB_HOST_Init();
while (1)
{
MX_USB_HOST_Process();
if(Appli_state == APPLICATION_READY)
{
[...]
}
}
}
[/code]
In addition to enabling VBUS
[code]
/**
* @brief Drive VBUS.
* @param phost: Host handle
* @param state : VBUS state
* This parameter can be one of the these values:
* 0 : VBUS Active
* 1 : VBUS Inactive
* @retval Status
*/
USBH_StatusTypeDef USBH_LL_DriverVBUS(USBH_HandleTypeDef *phost, uint8_t state)
{
/* USER CODE BEGIN 0 */
/* USER CODE END 0*/
if (phost->id == HOST_FS)
{
if (state == 0)
{
/* Drive high Charge pump */
/* ToDo: Add IOE driver control */
/* USER CODE BEGIN DRIVE_HIGH_CHARGE_FOR_FS */
HAL_GPIO_WritePin(OTG_PWR_OUT_GPIO_Port, OTG_PWR_OUT_Pin, GPIO_PIN_SET);
/* USER CODE END DRIVE_HIGH_CHARGE_FOR_FS */
}
else
{
/* Drive low Charge pump */
/* ToDo: Add IOE driver control */
/* USER CODE BEGIN DRIVE_LOW_CHARGE_FOR_FS */
HAL_GPIO_WritePin(OTG_PWR_OUT_GPIO_Port, OTG_PWR_OUT_Pin, GPIO_PIN_RESET);
/* USER CODE END DRIVE_LOW_CHARGE_FOR_FS */
}
}
HAL_Delay(200);
return USBH_OK;
}
[/code]
I'm reading the values but I do not know how to interpret them.
2019-04-19 2:12 AM
Hi engenharia4
can you tell me about your microsoft keyboard details!?
i run the code like above with microsoft curve 3000 keyboard but i cant get data form that and always return NULL!
I would appreciate for your answer
2019-04-22 4:27 AM
HI,
Take a look at this,
https://community.st.com/s/question/0D50X00009XkZ4KSAV/usb-host
for me, it was the answer,
I have followed changes proposed by @tsuneo , and got all keyboards working.
hope this helps.
Att.
2019-04-23 12:51 PM
thanks for your reply
you just exchange the HID_Handle->state = HID_IDLE; with HID_Handle->state = HID_SYNC;
then keyboards start to communicate?!
in my case it doesnt work, can you share your code!?
regards
2019-04-23 1:28 PM
code at main. c:
extern USBH_HandleTypeDef hUsbHostFS;
extern HID_KEYBD_Info_TypeDef keybd_info;
unsigned int output=0;
if(USBH_HID_GetDeviceType(&hUsbHostFS)==0x02)
{
output=USBH_HID_GetRAWCode(USBH_HID_GetKeybdInfo(&hUsbHostFS));
}
code at usb_hid.c:
/**
* @brief USBH_HID_Process
* The function is for managing state machine for HID data transfers
* @param phost: Host handle
* @retval USBH Status
*/
static USBH_StatusTypeDef USBH_HID_Process(USBH_HandleTypeDef *phost)
{
USBH_StatusTypeDef status = USBH_OK;
HID_HandleTypeDef *HID_Handle = (HID_HandleTypeDef *) phost->pActiveClass->pData;
switch (HID_Handle->state)
{
case HID_INIT:
HID_Handle->Init(phost);
HID_Handle->state = HID_SYNC; // skip HID_IDLE state
break;
case HID_IDLE:
if(USBH_HID_GetReport (phost,
0x01,
0,
HID_Handle->pData,
HID_Handle->length) == USBH_OK)
{
fifo_write(&HID_Handle->fifo, HID_Handle->pData, HID_Handle->length);
HID_Handle->state = HID_SYNC;
}
break;
case HID_SYNC:
/* Sync with start of Even Frame */
if(phost->Timer & 1)
{
HID_Handle->state = HID_GET_DATA;
}
#if (USBH_USE_OS == 1)
osMessagePut ( phost->os_event, USBH_URB_EVENT, 0);
#endif
break;
case HID_GET_DATA:
USBH_InterruptReceiveData(phost,
HID_Handle->pData,
HID_Handle->length,
HID_Handle->InPipe);
HID_Handle->state = HID_POLL;
HID_Handle->timer = phost->Timer;
HID_Handle->DataReady = 0;
break;
case HID_POLL:
if(USBH_LL_GetURBState(phost , HID_Handle->InPipe) == USBH_URB_DONE)
{
if(HID_Handle->DataReady == 0)
{
fifo_write(&HID_Handle->fifo, HID_Handle->pData, HID_Handle->length);
HID_Handle->DataReady = 1;
USBH_HID_EventCallback(phost);
#if (USBH_USE_OS == 1)
osMessagePut ( phost->os_event, USBH_URB_EVENT, 0);
#endif
}
}
else if(USBH_LL_GetURBState(phost , HID_Handle->InPipe) == USBH_URB_STALL) /* IN Endpoint Stalled */
{
/* Issue Clear Feature on interrupt IN endpoint */
if(USBH_ClrFeature(phost,
HID_Handle->ep_addr) == USBH_OK)
{
/* Change state to issue next IN token */
HID_Handle->state = HID_GET_DATA;
}
}
break;
default:
break;
}
return status;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.