2017-11-03 2:27 PM
Hi ST,
I have just downloaded 'STM32Cube_FW_F4_V1.17.0' and found it has 'libarm_cortexM7l_math.a' in CMSIS folder.
There is no cortexM4 file so I am confused if M7 library is compatible with M4.
I think this is a mistake because I can't seem to find any info on your release note about this.
I can use V1.16.0 M4 library instead of V1.17.0 M4 but I would use the new one if M4 lib has been updated.
Cheers.
Chris
2017-11-03 3:24 PM
>>
I think this is a mistake because I can't seem to find any info on your release note about this.
Would tend to agree. Just copy the files over from V1.16.0
2017-11-06 5:51 AM
Hello,
Thank you for your reported issue. I will raise this internally.
Best Regards
Imen
2017-11-07 11:30 PM
I don't think you actually need to copy the V1.16.0 libs over; I just added both the 1.17 and 1.16 library paths (in that order) to the library paths. Once we get an updated FW release with this fixed, I think I can just delete the library paths once updated.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.