2024-09-30 9:44 PM
Hello, I am in need of the SVD file for the newly released C071 model with USB. AFAICT they have not been posted or updated anywhere yet.
I'm working in Rust which requires the SVD file for generating register accessors so I cannot do anything with the chip until they are available.
Solved! Go to Solution.
2024-10-01 1:55 AM
2024-10-01 1:55 AM
2024-10-01 8:15 AM
Thank you very much!
2024-10-07 3:41 AM
Thanks for contributing on Rust for STM32C0 !
2024-10-18 10:16 AM
Thanks, I have now succeeded to establish USB Serial communications with C071 on the Rust/stm32-rs stack using the provided SVD files.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.