2015-10-29 6:03 AM
Hi all.
im about to work on a project which include an LCD as user interface and suppose to display images.LCD size is 240x320 pixels.im trying to use STeMWin tools - GUIBuilder and BMPCVT and FNTCVT.its seems like working.my first question is - what would be the best way to hold the images database(?), and using which format?(PNG, BMP, GIF)my second concern - during some tests with the tool and some small images, i used GUIBuilder to create some image (for start, only text), and after calling the function created by GUIBuilder, i used one of the functions GUI_Delay() or GUI_Exec() to update the LCD buffer and when using those functions the image get blurred for about a half second. is there any way to overcome that issue? why is that happening (only text was created).thanks for any help.2015-11-06 2:32 AM
Hi Assaf,
I will respond to the first question as I think that the second one is already asked in this [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/STemWin%20AN4323%20clock%20enable%20issue&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21¤tviews=28]thread.So, The use of PNG,BMP or GIF depends on application requirements:1-GIF is an animated image,2-PNG is a compressed image with transparency (for decoding, the library libpng must be added)3-BMP is an image without compression which means saving in time but loss of memory.By consequence, you have to choose one of them according to needs. -Shahrzad-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.