2013-01-25 12:47 PM
Hi,
Just opened a STM3240G-EVAL kit. I'm trying to get the STM32F2-F4 Demonstration Builder to run, without much success. If I download the prebuilt binary ''STM324xG_EVAL_Demonstration_Builder_V1.3.0.hex'', it runs until I tap an ICON, then it crashes. If I download the prebuilt binary ''STM324x7I_EVAL_Demonstration_Builder_V1.3.0.hex, it runs fine. Surprising, since this seems like the wrong CPU. The box says this should have a STM32F407IGH6 part, but the chip says STM32F457IGH6. So, which is the correct target for this board? Why does the chip say ''457''? I have a full IAR license, and can rebuild the STM324xG-EVAL project in IAR, and it ends up in the hard fault handler. There is also a STM324x7I-EVAL project in IAR, but it won't build, since it specifies a STM32F437II processor, which doesn't seem to be supported yet by IAR. Any suggestions? Thanks #stm32-demonstration-builder2013-01-25 3:38 PM
From Rev 1 of UM1461
''1.1 Features■ STM32F407IGT6 microcontroller. The MCU marking on the first boards manufactured is STM32F457IGH6.'' I'd just go with the 407IG as the target. There are a bunch of reasons why it might Hard Fault, most likely that the FPU is not enabled, but FPU instructions are encountered. Use the debugger or a better fault handler and determine the address of the faulting code. The FPU enabling code is typically in the front of SystemInit()
2013-01-28 5:42 AM
Thanks for that little tidbit from Rev 1 of the manual - My copy of the manual, Rev 4, doesn't have that.
Sure, I can debug this thing, it's just kind of surprising that a demo doesn't run out-of-the box.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.