2011-04-08 3:59 AM
STM3210E-Eval uClinux Problem
2011-05-17 5:31 AM
Hi Podany,
Can you remove the LCD, and try again. Let me know if it is ok? Regards, STOne.2011-05-17 5:31 AM
Hi STOne,
I removed the LCD and it worked! thx for the hint. But could you explain why this happens and what to do about it? I don't need the LCD now, but maybe in the future. I also tried to get the jffs version of uClinux to run. But when I install the bootloader (kernel_boot_loader.hex) via RS232 and then try to connect via USB like I did with the tiny bootloader, the board doesn't respond (it's not detected as a usb-device). Is this problem linked to the LCD problem? Regards, max
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.