2018-01-18 6:28 AM
I am working with the STM32091C-Eval board trying to see how the touch pads work. I have selected the TSC example code and gone to build the code using TrueStudio. I receive the following error message:
08:27:19 **** Rebuild of configuration Debug for project STM32091C_EVAL ****
Info: Internal Builder is used for buildarm-atollic-eabi-gcc -c ..\..\..\..\..\..\..\..\Drivers\STM32F0xx_HAL_Driver\Src\stm32f0xx_hal_rcc_ex.c -mthumb -mcpu=cortex-m0 -std=gnu11 -DSTM32F091xC -DUSE_HAL_DRIVER -DUSE_STM32091C_EVAL -I../../../Inc -I../../../../../../../../Drivers/CMSIS/Device/ST/STM32F0xx/Include -I../../../../../../../../Drivers/STM32F0xx_HAL_Driver/Inc -I../../../../../../../../Drivers/BSP/STM32091C_EVAL -I../../../../../../../../Drivers/BSP/Components/Common -I../../../../../../../../Utilities/Log -I../../../../../../../../Utilities/CPU -I../../../../../../../../Drivers/CMSIS/Include -Os -ffunction-sections -g3 -fstack-usage -Wall -fmessage-length=0 -Wno-strict-aliasing -specs=nano.specs -o Drivers\STM32F0xx_HAL_Driver\stm32f0xx_hal_rcc_ex.o arm-atollic-eabi-gcc: error: ..\..\..\..\..\..\..\..\Drivers\STM32F0xx_HAL_Driver\Src\stm32f0xx_hal_rcc_ex.c: No such file or directoryarm-atollic-eabi-gcc: fatal error: no input filescompilation terminated.The file is in the code display under STM32F0xx_HAL_Driver and I found the location of the code on my hard drive. I don't know why I have the error.
2018-01-18 7:25 AM
I would try to correct paths settings:
'stm32f0xx_hal_rcc_ex.c: No such file or directory'
2018-01-18 7:29 AM
The file does show up in the 'Project Explorer' panel.
So how do I correct the paths settings? I am new to this development system and need help in finding these items.
2018-01-18 7:40 AM
I would try to re-add them (remove then add) - I use Keil where files are marked when in project panel but not accessible.
Maybe you have another process blocking this file (locked by hanging process?)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.