2012-02-15 9:56 AM
Hello.
Sorry my english language -- i am russian.I am develop design with use microcontroller STM32F107.I solve use USB connection, as USB CDC.Find and download example of this implementation.I learn some and i have some questions.(sorry if roughly, i don`t know how right assembler sentence).1. How can i know, when i can repeat transfer(from mc to PC) (i think that callback function EP1_IN_Callback() is called when data was transfered, but ...).2. I think, that, if data is resived, callback function EP3_OUT_Callback() call. Is it true?3. I realize some example: i transfer one any digital from PC to COM3 (STM32 OTG_FS), then callback function EP3_OUT_Callback() is called, where i set flagf_Zapros = 1. Main program check this flag and flag fReady_to_Write then, if true, call function USB_SIL_Write(). That is i want start IN transfer (from mc to PC) after recive requestfrom PC. But... When i test this idea(PC transmiter - programm Terminal v.1b) PC buzz( don`t ansver on action). Example: main.c fZapros = 0; fReady_to_Write = 1; offset = 0; while(1) { if(fZapros) { if(fReady_to_Write) { fReady_to_Write = 0; USB_SIL_Write(EP1_IN, &USB_Tx_Buffer[0] + offset, 1); offset += 64; if(offset >= NumPoint) fZapros = 0; } }Flag fReady_to_Write i set in callback function EP1_IN_Callback().offset - for transfer data whith size more than 64 bytes.NumPoint - number bytes, which will be transfer.(for example 1024). If can, help please.2012-02-16 7:33 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.