2014-07-01 3:40 AM
Hello,
I'm using a STM32F30x as a Slave. The Master is a custom board that select/deselect the Slave by toggling an output pin. In the Slave side i configured the SPI with hardware management, SPI_InitStructure.SPI_NSS = SPI_NSS_Hard; There is no difference when it's managed by software SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; Someone could have an idea what the difference ?Thanks in advance2014-07-07 6:48 AM
Is there always the problem of Hardware CS with STMF3?
I tried to manage it but no success. Someone made it work ?2014-07-07 8:34 AM
Hi,
I'm using STM-L1 and not STM-F3 as SPI slave with hardware CS, but I think this can help.I defined the NSS pin in the STM-L1 (SPI slave) as external interrupt with trigger falling. This EXTI indicate the master select the CS and ready to transfer SPI data.2014-07-14 10:46 AM
Thank you rogel.zohar for your help.
I did the same as you but the problem is that there is no difference between:SPI_InitStructure.SPI_NSS = SPI_NSS_Hard; and SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;For me a hardware CS is when we don't need to use an external interrupt to detect it. It should operate automatically. May be I make a mistake about the CS stuff. Someone can highlight this point please ?B.R
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.