2024-01-17 5:33 AM - last edited on 2024-01-17 5:57 AM by Imen.D
Recently working with spi communication in stm32g070rb using stm32CubeIDE (HAL library).SPI master receive interrupt triggered continuosly when there is no interrupt.But same code wrote in SPI slave its works perfectly.I also put Pull down resistor.Please provide solution
Solved! Go to Solution.
2024-01-17 5:46 AM
Please follow SPI examples in the CubeMX repository to understand how they function. Here is one of several:
2024-01-17 5:46 AM
Please follow SPI examples in the CubeMX repository to understand how they function. Here is one of several:
2024-01-17 9:18 PM
I already ssen this example so My main problem is if i configure SPI master Spi rx callback automatically triggered again and again. Slave devices that rx callback function works perfectly. I think if any master mode fault what reason master spi interrupt triggered unwantedly
2024-01-17 9:45 PM
i have also one doubt if any did not connect miso,mosi,sclk pins to slave devices. i just load the code to master device then i see interrupt rx callback or error occurs. pls provide solution
this code works properly in full duplex slave if i set full duplex master or half duplex master does not works
my clock configuration is perfectly set and also give interrupt priority why this only woks slave not master devices
int main(void)
{
HAL_Init();
SystemClock_Config();
HAL_SPI_Receive_IT(&hspi1,spi_data,1);
while (1)
{
}
}
void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)
{
HAL_SPI_Receive_IT(&hspi1,spi_data,1); // ready for new interrupt
}
2024-01-18 6:14 AM
Please don't duplicate post. It creates more work for people here. Stick to one thread.
2024-01-18 9:47 PM
sorry for inconvinence and thank for your patience
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.