2016-06-21 2:22 AM
I'm facing with a problem regarding debug session.
When I start debug session, after the configuration of USART2 the debug session is closed.
Keil message:
Cannot access target. Shutting down debug session
The shutdown occur with this instruction:
__HAL_AFIO_REMAP_USART2_ENABLE();
This is my configuration:
Without debug the board works well, but I need the debug to solve some bug.
Thanks!
2016-06-21 5:43 AM
And what does the code in that function actually do? Step into it.
Confirm AFIO and GPIOD clocks are enabled.2016-06-21 6:02 AM
Hi clive1,
The code execute this macro/**
* @brief Enable the remapping of USART2 alternate function CTS, RTS, CK, TX and RX. * @note ENABLE: Remap (CTS/PD3, RTS/PD4, TX/PD5, RX/PD6, CK/PD7) * @retval None */ #define __HAL_AFIO_REMAP_USART2_ENABLE() SET_BIT(AFIO->MAPR, AFIO_MAPR_USART2_REMAP) GPIOD clock is enabled by this macro:__HAL_RCC_GPIOD_CLK_ENABLE();
This is the UART2 Init function:/* USART2 init function */
static void MX_USART2_UART_Init(void) { huart2.Instance = USART2; huart2.Init.BaudRate = 115200; huart2.Init.WordLength = UART_WORDLENGTH_8B; huart2.Init.StopBits = UART_STOPBITS_1; huart2.Init.Parity = UART_PARITY_NONE; huart2.Init.Mode = UART_MODE_TX_RX; huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart2.Init.OverSampling = UART_OVERSAMPLING_16; if (HAL_UART_Init(&huart2) != HAL_OK) { Error_Handler(); } } Inside the Init function there is this function's call to: /* Init the low level hardware */ HAL_UART_MspInit(huart); This function initialize the low level of UART2:else if(huart->Instance==USART2)
{ /* USER CODE BEGIN USART2_MspInit 0 */ /* USER CODE END USART2_MspInit 0 */ /* Peripheral clock enable */ __HAL_RCC_USART2_CLK_ENABLE(); /**USART2 GPIO Configuration PD5 ------> USART2_TX PD6 ------> USART2_RX */ GPIO_InitStruct.Pin = Debug_Serial_TX_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; HAL_GPIO_Init(Debug_Serial_TX_GPIO_Port, &GPIO_InitStruct); GPIO_InitStruct.Pin = Debug_Serial_RX_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(Debug_Serial_RX_GPIO_Port, &GPIO_InitStruct); //__HAL_AFIO_REMAP_USART2_ENABLE(); /* Peripheral interrupt init */ HAL_NVIC_SetPriority(USART2_IRQn, 0, 0); HAL_NVIC_EnableIRQ(USART2_IRQn); /* USER CODE BEGIN USART2_MspInit 1 */ /* USER CODE END USART2_MspInit 1 */ } And here the debug session fails.2016-06-21 7:50 AM
Are you sure you don't have an issue externally with PD5? Could you scope the NRST pin and see what that does.
You could perhaps set the pin up as a GPIO and drive it high and low to see if that precipitates the same failure.2016-06-22 12:25 AM
Hi clive1
I have the same problem. It seems that when I try to set a bit in AFIO->MAPR (for example AFIO->MAPR |= 0x30; the debug session fails. Do you have any idea why it fails? Thanks2016-06-22 12:57 AM
Hi clive1,
The GPIO PD5 in directly connected to an FTDI converter. Same thing for GPIO PD6.There aren't any components along these wires.This morning I will scope the NRST line to see what happen.Could this issue related to the remapping of UASART2 on PD5 and PD6?Thanks for your time.2016-06-22 1:19 AM
Hi,
I found a temporary solution for you. You should useAFIO->MAPR |= AFIO_MAPR_USART2_REMAP | AFIO_MAPR_SWJ_CFG_JTAGDISABLE;
(in case of using SW) instead of using
__HAL_AFIO_REMAP_USART2_ENABLE();
I wonder if anyone can explain why the AFIO->MAPR value after the execution of following code is 0x04000030?!?
AFIO->MAPR = 0x02000000UL | 0x30; // The AFIO->MAPR value is 0x04000030 after execution of this line!!!
Bests,
Misagh
2016-06-24 4:33 AM
Thanks Misagh92!
Your solution works! Now I can debug and read output form UART2.The only problem is connected to code generation performed by ST CubeMX. When I generate the project's code the__HAL_AFIO_REMAP_USART2_ENABLE()
is restored.
But this is not a big problem. Just keep it in mind.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.