2024-06-12 5:27 PM
i am using a stm32f401ccu6 board to receive modbus rtu requests from a master device(windows laptop running simplymodbus) and prepare the response buffer and send it
so far i can see that the response buffer is being prepared as expected in the live expressions table, however whenever i am trying to send the message back to the master it is receiving the message with FF and 00 values at the beginning and end of the response
for example if the response is 07 03 04 57 73 7A then the master is receiving FF 07 03 04 57 73 7A 00
also i am using a rs485 transceiver along with the uart lines and the hardware seems to be working fine as when i programmed the stm32 to be the master and the pc to be the slave it was working perfectly fine
what could be the issue
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.