cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Nucleo-144 (413ZH) USART_2 Printf

jkasper
Associate II

Hello!

I am running the UART_Printf example on my Nucleo and the output to USART3 (default) works fine, but when I change the output to USART2 or USART6, it doesn't send data.

1 ACCEPTED SOLUTION

Accepted Solutions

Ok, but that sounds like a coding or configuration issue, both those USARTs should be functional.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

3 REPLIES 3

Ok, but that sounds like a coding or configuration issue, both those USARTs should be functional.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

OK thanks, I see the configuration in main.h in the example.

JackChien
Associate

Refer UM1974

6.9 USART communication
The USART3 interface available on PD8 and PD9 of the STM32 can be connected either to
ST-LINK or to ST morpho connector. The choice is changed by setting the related solder
bridges. By default the USART3 communication is enabled between the target STM32 and
both the ST-LINK and the ST morpho connector.

Board design only support USART3 for ST-LINK

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.