2014-06-11 2:06 PM
Hi,
I am familiar with Standard Pheripheral Library on STM32F100 MCU. ==== The problem is that on nucleo-053 (SPL is not available for this MCU) I cannot make USART working properly. I generated the code using CubeMX 4.2 (USART2 enabled, NO parity, 1 stopbit, 8 data bits). When I use the following piece of code: uint8_t pData[40]; int k; for(k=0;k<40;k++){pData[k]=48+k;} HAL_UART_Transmit(&huart2, pData, 40, 10); only numbers and @ are sent correctly. Letters ('abcd', etc ) are displayed as if they have extended ASCI codes (extra bit was added in front of the original code making it extended code). I know that for 9B & parity the HAL driver plays this way. But it's not the cae, I guess (no 9B & parity). I do not use physical uart port - Virtual COM is used (ST-link 2.1 feature). === Anyway, could you please share USART code example for nucleo-L053? Thanks, BogdanSolved! Go to Solution.
2014-06-30 6:11 AM
Hi bogdan,
You can download the STM32CubeL0 FW package from here: UART examples are available under: Projects\STM32L053R8-Nucleo\Examples\UARTWith regards.2014-06-30 6:11 AM
Hi bogdan,
You can download the STM32CubeL0 FW package from here: UART examples are available under: Projects\STM32L053R8-Nucleo\Examples\UARTWith regards.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.