2025-07-30 11:20 AM
Hi there
Is there any stm32 MCU versions that has can run both CAN and USB simultaneously without conflicting with the PB8 boot pin? Also the USB will only be recognized if the PB8 pin is pulled high can i just directly connect it to 3.3v and always keep it on. will that be a problem
Solved! Go to Solution.
2025-07-30 12:56 PM
Yeah i tried USB CDC in STM32G4 it worked but still i need to pull the BOOT pin high while connecting the USB. is there a way i can bypass that. i just need to connect the USB to my PC and start sending/receiving messages.
2025-07-30 1:03 PM
No, you should not have to pull the boot pin high to get CDC to work. Something is amiss.
2025-07-30 8:04 PM
So i don't have to do anything for USB CDC if just connect USB To my SMT32 it will show as a USB VCP?
2025-08-05 3:47 AM
Hi @kavinkumar
You can follow this example, You don't need to pull any boot pin to enumerate as VCP.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.