2015-12-23 6:24 AM
hi, i'm currently learning how to program mcu by means of stm32+cubemx+hal, and i stuck with i2c interface, trying to write a byte to eeprom at24c04 with function
HAL_I2C_Mem_Write(&hi2c1, 0x50, 0x00, 8, &number, 8, 20); * @param hi2c: pointer to a I2C_HandleTypeDef structure that contains * the configuration information for I2C module * @param DevAddress: Target device address * @param MemAddress: Internal memory address * @param MemAddSize: Size of internal memory address * @param pData: Pointer to data buffer * @param Size: Amount of data to be readam i doing it right?Tried expression if(HAL_I2C_IsDeviceReady(&hi2c1, 0x50, 20, 500) == HAL_ERROR) HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);led turns on immediately. ic connected accordingly to datasheet.will gladly appreciate any information about my problemWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.