2010-07-08 3:52 AM
STM32 I2C 2nd ReadByte (can't GenerateStart)
2011-05-17 4:58 AM
Does not anyone a suggestion?
2011-05-17 4:58 AM
I think you shouldn't have the STOP in the middle of your routine and I'm not sure about the ACK disable.
Your code looks similar to some I use to read another I2C device with device address, register number and byte read(s) - which seems to work. Does it help you? John F. #define DeviceAddress 0xCE void DeviceReadBuffer(uint8_t* pBuffer, uint8_t NumByteToRead) { /*!< While the bus is busy */ while(I2C_GetFlagStatus(I2C1, I2C_FLAG_BUSY)) { } /*!< Send START condition */ I2C_GenerateSTART(I2C1, ENABLE); /*!< Test on EV5 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT)) { } /*!< Send EEPROM address for write */ I2C_Send7bitAddress(I2C1, LTC4151Address, I2C_Direction_Transmitter); /*!< Test on EV6 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)) { } //send the reg select COMMAND byte I2C_SendData(I2C1, 0); /*!< Test on EV8 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED)) { } //send START condition a second time I2C_GenerateSTART(I2C1, ENABLE); /*!< Test on EV5 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT)) { } /*!< Send EEPROM address for read */ I2C_Send7bitAddress(I2C1, LTC4151Address, I2C_Direction_Receiver); /*!< Test on EV6 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_RECEIVER_MODE_SELECTED)) { } /*!< While there is data to be read */ while(NumByteToRead) { if(NumByteToRead == 1) { /*!< Disable Acknowledgement */ I2C_AcknowledgeConfig(I2C1, DISABLE); /*!< Send STOP Condition */ I2C_GenerateSTOP(I2C1, ENABLE); } /*!< Test on EV7 and clear it */ if(I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_RECEIVED)) { /*!< Read a byte from the EEPROM */ *pBuffer = I2C_ReceiveData(I2C1); /*!< Point to the next location where the byte read will be saved */ pBuffer++; /*!< Decrement the read bytes counter */ NumByteToRead--; } } /*!< Enable Acknowledgement to be ready for another reception */ I2C_AcknowledgeConfig(I2C1, ENABLE); }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.