2016-01-07 3:14 AM
Hi, similar (but different) issue to a previous posting of mine.
I am seeing PA1 on an STM32F205 get driven low during standby after __WFI() I was expecting all GPIO to go Hi-Z during standby apart from the pins detailed in the datasheet (and SWD/JTAG pins when sleep-debugging is enabled). I thought it might be an issue with clocks being disabled before sleep so I am now manually changing PA1 to an input before standby (it's used as an output in my design). There is an external 10K pull-up on PA1, but it still gets driven to 0v during standby. If I dont enable debug sleep, then the pin behaves as expected, but if I call DBGMCU_Config(DBGMCU_STANDBY, ENABLE); before standby, I see this behaviour. Thanks in advance for any tips. Jamie.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.