2013-05-09 7:53 AM
Attached are two logic analyzer traces. You can download the software to view them from here:
What you see is that when I use the flash loader demonstrator tool, the connection fails. It fails for the following reason. The bootloader is not correctly determining the baud-rate. The bootloader is sending 0x7F at 115200 bps, but the bootloader configures itself as approximately 11000 bps.When I use my own flash loader you can see that the bootloader correctly configures itself as 115200bps.The particular processor I am targetting is the STM32F205ZCFrom what I can tell the only difference is that for the ST-tool the TX line goes high only 600us before the 0x7f is sent. In my case the TX line goes high long before the 0x7f is sent.Is there a fix for this from ST?I am using version 2.6.0 of the flash loader demonstrator from Nov 2012.Note: in my traces the boot0 and reset lines are inverted polarity from the data sheet.2013-05-09 10:11 AM
Is there a fix for this from ST?
It's in ROM, it is what it is. It tests for the auto-baud data pattern once after reset. Make sure you're using 8-bit Even parity. For an STM32 this would require 9-bit mode. Export your plots in PDF, JPG or PNG, something web friendly.2013-05-09 10:38 AM
Here are pictures if that helps.
I realize the bootloader is in ROM, but it is the same bootloader in both cases. The only difference that I can surmise that accounts for the different behavior is the way the host drives the TX line. ________________ Attachments : Flash_Downloader_Tool_Failure_to_Connect.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0wC&d=%2Fa%2F0X0000000bfq%2FqdsB7FHvHvAVM8izMDjRanWpJWUrqKxZKcOcgBa_cKA&asPdf=falsePersonal_Downloader_Tool_Success_to_Connect.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0w7&d=%2Fa%2F0X0000000bfr%2FCQfbYATCdVBgFg04URaLj4zw5BQ.3W6qWcqrP5au2Dw&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.