2018-07-10 6:37 AM
Hi,
Ineed to create firmware on STM32F417VGT to act as an TCP server and to accept multiple connection at the same time.
Project is generated using CubeMX.
I have default task
void StartDefaultTask(void const * argument)
{
/* init code for LWIP */
MX_LWIP_Init();
/* USER CODE BEGIN StartDefaultTask */
struct netconn *conn, *in_conn;
err_t err, accept_err;
struct netbuf *buf;
uint16_t len;
char echoBuff[100];
conn = netconn_new(NETCONN_TCP);
if (conn != NULL)
{
err = netconn_bind(conn, IP_ADDR_ANY, 4001);
if (err == ERR_OK)
{
netconn_listen(conn);
while (1)
{
accept_err = netconn_accept(conn, &in_conn);
if (accept_err == ERR_OK)
{
len = sprintf(echoBuff, 'netconn_accept - OK\r\n');
HAL_UART_Transmit(&huart2, (uint8_t*)echoBuff, len, 1000);
osThreadDef(netTask, StartNetTask, osPriorityIdle, 0, 128);
netTaskHandle = osThreadCreate(osThread(netTask), (void*)in_conn);
}
}
}
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
After each netconn_accept a new task is created to handle certain connection.
void StartNetTask(void const * argument)
{
/* USER CODE BEGIN StartNetTask */
struct netconn * nc = (struct netconn *)argument;
struct netbuf * nb;
char * buffer = pvPortMalloc(2048);
uint16_t len;
err_t err;
void *data;
char echoBuff[100];
sprintf(buffer, 'Hello from STM\r\n');
netconn_write(nc, buffer, strlen(buffer), NETCONN_COPY);
/* Infinite loop */
while (netconn_recv(nc, &nb) == ERR_OK)
{
do
{
netbuf_data(nb, &data, &len);
netconn_write(nc, data, len, NETCONN_COPY);
}
while (netbuf_next(nb) >= 0);
}
err = netconn_close(nc);
if (err == ERR_OK)
{
len = sprintf(echoBuff, 'netconn_close - OK\r\n');
HAL_UART_Transmit(&huart2, (uint8_t*)echoBuff, len, 1000);
}
err = netconn_delete(nc);
if (err == ERR_OK)
{
len = sprintf(echoBuff, 'netconn_delete - OK\r\n');
HAL_UART_Transmit(&huart2, (uint8_t*)echoBuff, len, 1000);
}
len = sprintf(echoBuff, 'Deleting current NetTask\r\n');
HAL_UART_Transmit(&huart2, (uint8_t*)echoBuff, len, 1000);
vTaskDelete(NULL);
/* USER CODE END StartNetTask */
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
What I need to implement is situation when the client is disconnected from server. In such a case I want to delete task that was created for this connection. Code for StartNetTask is not working as I require.
Is there any way how to solve this task?
Thank you
martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.