2015-05-26 11:50 AM
Intro
I am using the STM32 Discovery board to talk with sensor that receives and sends data packet on SPI1. I have unpopulated U5 on the discovery board so that it lets me use the SPI1 port. I can send the data packet (3 bytes of data accompanied by 2 bytes of modbusCRC16 checksum. The sensor receives the packet ok and sends data back in a similar packet. On implementing the checksum I found that none of the packets that i received were matching. On probing(literally) with a scope I found that the data on the scope did not match the memory (using KeilMDK debugger)Issue Last bit on certain bytes is carried or borrowed i.e. in a packet where the scope shows 04h, 00h,00h,30h,01h the memory shows 05h, 00h,00h,30h, 00h and is fairly consistent, another example is Scope : F0h,00h,00h,71h,F3h Memory: F1h,00h,00h,70h,F3h I know that there is a dummy byte that comes as zero when first read, however, i do not understand this. Kindly advise. spi.c void MX_SPI1_Init(void) { hspi1.Instance = SPI1; hspi1.Init.Mode = SPI_MODE_MASTER; hspi1.Init.Direction = SPI_DIRECTION_2LINES; hspi1.Init.DataSize = SPI_DATASIZE_8BIT; hspi1.Init.CLKPolarity = SPI_POLARITY_LOW; hspi1.Init.CLKPhase = SPI_PHASE_1EDGE; hspi1.Init.NSS = SPI_NSS_HARD_OUTPUT; // hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256; hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_64; hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi1.Init.TIMode = SPI_TIMODE_DISABLED; hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLED; HAL_SPI_Init(&hspi1); } void HAL_SPI_MspInit(SPI_HandleTypeDef* hspi) { GPIO_InitTypeDef GPIO_InitStruct; if(hspi->Instance==SPI1) { /* USER CODE BEGIN SPI1_MspInit 0 */ /* USER CODE END SPI1_MspInit 0 */ /* Peripheral clock enable */ __SPI1_CLK_ENABLE(); /**SPI1 GPIO Configuration PA5 ------> SPI1_SCK PA6 ------> SPI1_MISO PA7 ------> SPI1_MOSI PA15 ------> SPI1_NSS */ GPIO_InitStruct.Pin = GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7|GPIO_PIN_15; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_LOW; GPIO_InitStruct.Alternate = GPIO_AF5_SPI1; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /* USER CODE BEGIN SPI1_MspInit 1 */ /* USER CODE END SPI1_MspInit 1 */ } } void HAL_SPI_MspDeInit(SPI_HandleTypeDef* hspi) { if(hspi->Instance==SPI1) { /* USER CODE BEGIN SPI1_MspDeInit 0 */ /* USER CODE END SPI1_MspDeInit 0 */ /* Peripheral clock disable */ __SPI1_CLK_DISABLE(); /**SPI1 GPIO Configuration PA5 ------> SPI1_SCK PA6 ------> SPI1_MISO PA7 ------> SPI1_MOSI PA15 ------> SPI1_NSS */ HAL_GPIO_DeInit(GPIOA, GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7|GPIO_PIN_15); /* USER CODE BEGIN SPI1_MspDeInit 1 */ /* USER CODE END SPI1_MspDeInit 1 */ } } /* USER CODE BEGIN 1 */ void HAL_SPI_enable(SPI_HandleTypeDef *hspi) { if((hspi->Instance->CR1 &SPI_CR1_SPE) != SPI_CR1_SPE) { /* Enable SPI peripheral */ __HAL_SPI_ENABLE(hspi); } } uint8_t HAL_SPI_TxRx1Byte(SPI_HandleTypeDef *hspi, uint8_t TxData) { uint8_t RxData; static uint8_t firstEntryFlag = 0; /* Process Locked */ __HAL_LOCK(hspi); /* Check if the SPI is not enabled */ if((hspi->Instance->CR1 &SPI_CR1_SPE) != SPI_CR1_SPE) { /* Enable SPI peripheral */ __HAL_SPI_ENABLE(hspi); } hspi->Instance->DR = TxData; while (!SPI_FLAG_RXNE); RxData = hspi->Instance->DR; __HAL_UNLOCK(hspi); return RxData; }2015-05-26 10:13 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.