2021-07-07 11:04 AM
Hi, I am trying to communicate with other CAN devices on CAN BUS with STM32F103.
I have enabled "void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)" to receive message interrupt as highest priority and in main loop I am checking if I got the message to which I need to respond.
If I have a message to which I need to respond and TxMailboxes have free space, I respond from main loop like so:
if (HAL_CAN_GetTxMailboxesFreeLevel(&hcan) > 0)
{
if (HAL_CAN_AddTxMessage(&hcan, &TxMsg.Header, data, &TxMailbox) != HAL_OK)
{
Error_Handler();
}
}The problem I am having is that "HAL_CAN_AddTxMessage" return "HAL_OK", but often (something like 50/50 chance) other devices do not get the message. So message gets lost? Why adding TxMessage could fail? And why don't I get any indication that it failed?
How to correctly send CAN BUS message without loosing it?
Solved! Go to Solution.
2021-07-07 12:12 PM
I have enabled AutoRetransmission feature. It seems to work much better now. Not sure if 100% sending rate, will need to test more.
2021-07-07 12:12 PM
I have enabled AutoRetransmission feature. It seems to work much better now. Not sure if 100% sending rate, will need to test more.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.