2009-02-10 8:16 PM
STM32 and system bus
2011-05-17 4:02 AM
Hello all,
I need to interface a CS8900 to STM32, so i need to use the system bus. Can I use the system bus unused pins as GPIOs? Thanks, Lorenzo2011-05-17 4:02 AM
If you'r gonna to interface ISA interface with STM32 through the FSMC, any unused pin either address or data signals can be used as GPIO :o
2011-05-17 4:02 AM
Quote:
On 11-02-2009 at 00:07, Anonymous wrote: If you'r gonna to interface ISA interface with STM32 through the FSMC, any unused pin either address or data signals can be used as GPIO :o Thank you! LWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.