2018-04-24 3:30 AM
Hi, I am trying to configure USART3 on STM324-Discovery for
asynchronous
communication. As i am configuring U(S)ART so I imported USART HAL libraries not UART libraries. But when i program USART with HAL_Usart_init function, the HAL_Usart_Receive() seems to be always receiving i.e. there is always some data in DR register. but when i do it with HAL_Uart_Init(), every thing seems to be working OK. The reference manual doesn't mention that HAL_USART_Init function can't be used for asynchronous communication.However
https://community.st.com/0D50X00009XkYJ8SAN
port mentions:- For HAL use, in order to use USART2 in Asynchronous mode, you should use
HAL_UART
_xxx APIs, with USART2 instance.
Is it true? Is there a reason behined?
I looked back into background register settings. both methods configure registers similarly except the OVER8 bit which is enabled in HAL_Usart_Init() function.
#kit-stm32f4-discovery #hal-usartWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.