2016-11-28 5:29 AM
Hello,
I have a problem with my application based on STemWin lib 5.32. Without WM_SetCreateFlags(WM_CF_MEMDEV) works very fine but there is some flikering. After activation of use memory device 1-2 minuts program is halted. How to avoid it? regards,PD2016-11-28 5:56 AM
Hello,
Are you following the user manual about WM_SetCreateFlags (WM_CF_MEMDEV)''The flag WM_CF_MEMDEV is frequently used to enable Memory Devices on all windows.Setting create flags is permitted before GUI_Init() is called. This causes the backgroundwindow to be also affected by the create flags.''Regards2016-11-28 6:18 AM
Hi,
yes I read this issue. Please see my ''main'':int main(void){ /* STM32F4xx HAL library initialization: - Configure the Flash prefetch, instruction and Data caches - Configure the Systick to generate an interrupt each 1 msec - Set NVIC Group Priority to 4 - Global MSP (MCU Support Package) initialization */ HAL_Init(); /* Configure the system clock to 180 Mhz */ SystemClock_Config(); MX_GPIO_Init(); MX_DMA_Init(); // !!! by PD MX_I2C3_Init(); // !!! by PD MX_I2C1_Init(); // !!! by PD MX_TIM1_Init(); // !!! by PD MX_TIM3_Init(); // !!! by PD MX_TIM4_Init(); // !!! by PD MX_TIM8_Init(); // !!! by PD MX_USART1_Init(); // !!! by PD MX_FMC_Init(); // !!! by PD FT5206_CTP_BSP_PB_Init(); // !!! by PD MX_RTC_Init(); // !!! by PD /***********************************************************/ HAL_TIM_Base_Start_IT(&htim1); HAL_TIM_Base_Start_IT(&htim3); HAL_TIM_Base_Start_IT(&htim4); HAL_TIM_Base_Start_IT(&htim8); /***********************************************************/ VARIABLE_INIT(); /* Init the STemWin GUI Library */ BSP_SDRAM_Init(); /* Initializes the SDRAM device */ __CRC_CLK_ENABLE(); /* Enable the CRC Module */ GUI_Init(); BSP_Config(); GUI_Initialized = 1; /* Activate the use of memory device feature */ //WM_SetCreateFlags(WM_CF_MEMDEV); //here is commented MainTask(); while (1) { }}WM_SetCreateFlags(WM_CF_MEMDEV) is after GUI_INIT.I have STM32F429BIT6 and 4 windows , rest (8) are created and deteted when aplication needs. regards,PDWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.