2018-12-18 7:47 PM
Hi everyone!
I'm in a hurry, I have a canbus network working with stm32F4 without problems working in STD Periph drivers, and even I have 2 sTM32F0 working HAL Can with out problems (I'm gonna left the 2 config), when I try to conect both networks, the CAN_H and CAN_L goes high, I can see in osciloscoe, the signal, when I connect the F0 to F4 network this happens, I cannot see whats wrong, please some advice?
this is the STM32F407 CANbus config with STD periph Drivers, I get those values from this web page from (http://www.bittiming.can-wiki.info) with a sample point of 87.5% Bit Rate = 125 and Clock rate of 42Mhz based in configuration
NVIC_IRQChannel = CAN1_RX0_IRQn;
RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE)
CAN_FilterInitStructure.CAN_FilterNumber = 13;
CAN_DeInit(CANBUSx);
CAN_InitStructure.CAN_TTCM = DISABLE;
CAN_InitStructure.CAN_ABOM = DISABLE;
CAN_InitStructure.CAN_AWUM = DISABLE;
CAN_InitStructure.CAN_NART = DISABLE;
CAN_InitStructure.CAN_RFLM = DISABLE;
CAN_InitStructure.CAN_TXFP = DISABLE;
CAN_InitStructure.CAN_Mode = CAN_Mode_Normal;
CAN_InitStructure.CAN_SJW = CAN_SJW_1tq;
CAN_InitStructure.CAN_BS1 = CAN_BS1_13tq;
CAN_InitStructure.CAN_BS2 = CAN_BS2_2tq;
CAN_InitStructure.CAN_Prescaler = 21;
CAN_Init(CANBUSx, &CAN_InitStructure);
CAN_FilterInitStructure.CAN_FilterFIFOAssignment = CAN_FIFO;
CAN_FilterInitStructure.CAN_FilterMode = CAN_FilterMode_IdMask;
CAN_FilterInitStructure.CAN_FilterScale = CAN_FilterScale_16bit;
CAN_FilterInitStructure.CAN_FilterIdHigh = 0x0000;
CAN_FilterInitStructure.CAN_FilterIdLow = 0x0000;
CAN_FilterInitStructure.CAN_FilterMaskIdHigh = 0x0000;
CAN_FilterInitStructure.CAN_FilterMaskIdLow = 0x0000;
CAN_FilterInitStructure.CAN_FilterFIFOAssignment = CAN_FIFO_ID;
CAN_FilterInitStructure.CAN_FilterActivation = ENABLE;
CAN_FilterInit(&CAN_FilterInitStructure);
NVIC_InitStructure.NVIC_IRQChannel = NVIC_IRQChannel;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 255;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x00;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
//FIFO
CAN_ITConfig(CANBUSx, CAN_IT_FMP0, ENABLE);
CAN_ITConfig(CANBUSx, CAN_IT_FMP1, ENABLE);
CAN_ITConfig(CANBUSx, CAN_IT_FF0, ENABLE);
CAN_ITConfig(CANBUSx, CAN_IT_FF1, ENABLE);
CAN_ITConfig(CANBUSx, CAN_IT_FOV0, ENABLE);
CAN_ITConfig(CANBUSx, CAN_IT_FOV1, ENABLE); And this is the configuracion of STM32F042 based in HAL drivers with a sample point of 87.5% Bit Rate = 125 and Clock rate of 48Mhz based in configuration
CAN_FilterConfTypeDef sFilterConfig;
static CanTxMsgTypeDef TxMessage;
static CanRxMsgTypeDef RxMessage;
hcan.Instance = CAN;
hcan.Init.Mode = CAN_MODE_NORMAL;
hcan.Init.SJW = CAN_SJW_1TQ;
hcan.Init.BS1 = CAN_BS1_13TQ;
hcan.Init.BS2 = CAN_BS2_2TQ;
hcan.Init.Prescaler = 24;
hcan.Init.TTCM = DISABLE;
hcan.Init.ABOM = ENABLE;
hcan.Init.AWUM = ENABLE;
hcan.Init.NART = DISABLE;
hcan.Init.RFLM = DISABLE;
hcan.Init.TXFP = DISABLE;
if (HAL_CAN_Init(&hcan) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
hcan.pTxMsg = &TxMessage;
hcan.pRxMsg = &RxMessage;
/*##-2- Configure the CAN Filter ###########################################*/
sFilterConfig.FilterNumber = 0;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig.FilterIdHigh = 0x0000;
sFilterConfig.FilterIdLow = 0x0000;
sFilterConfig.FilterMaskIdHigh = 0x0000;
sFilterConfig.FilterMaskIdLow = 0x0000;
sFilterConfig.FilterFIFOAssignment = 0;
sFilterConfig.FilterActivation = ENABLE;
sFilterConfig.BankNumber = 14;
if (HAL_CAN_ConfigFilter(&hcan, &sFilterConfig) != HAL_OK)
{
/* Filter configuration Error */
Error_Handler();
}
hcan.pTxMsg->StdId = 0x321;
hcan.pTxMsg->ExtId = 0x00;
hcan.pTxMsg->RTR = CAN_RTR_DATA;
hcan.pTxMsg->IDE = CAN_ID_STD;
hcan.pTxMsg->DLC = 8;
hcan.pTxMsg->Data[0] = 0x40;
hcan.pTxMsg->Data[1] = 0x41;
hcan.pTxMsg->Data[2] = 0x42;
hcan.pTxMsg->Data[3] = 0x43;
hcan.pTxMsg->Data[4] = 0x44;
hcan.pTxMsg->Data[5] = 0x45;
hcan.pTxMsg->Data[6] = 0x46;
hcan.pTxMsg->Data[7] = 0x47; Both networks are working with interruptions, working well canbus F4 network without problems and canbus F0 network without problems, I dont know if this ir enough to detect a problem, if you need my MCU initialization I can upload it, or even any part of my code, I need to communicate those two, I CANNOT change to hal in F4 (Because that MCU are in a product already) and with F0 I need to use HAL (Because of the project).
Any help would be appreciated.
2018-12-18 8:43 PM
Ok! I was able to get to the error, just in case someone has the same problem. in STM32F407 canbus initialization:
// From
CAN_FilterInitStructure.CAN_FilterNumber = 13;
//To
CAN_FilterInitStructure.CAN_FilterNumber = 0; //From
CAN_FilterInitStructure.CAN_FilterScale = CAN_FilterScale_16bit;
//To
CAN_FilterInitStructure.CAN_FilterScale = CAN_FilterScale_32bit;I'v got this parameter twice assigned to " different parameters:
CAN_FilterInitStructure.CAN_FilterFIFOAssignment = 0;Changing that, everything was working!
2020-05-27 2:53 AM
hello, i am facing the same problem rn! is it possible for u to send me the code after working? it would be really great if u did. thank u
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.