2009-08-18 4:08 AM
Start a program in RAM?
2011-05-17 4:20 AM
I have an application in FLASH. I want it to be able to download a program to SRAM and then execute it.
What traps or pitfalls do I have to think about? I have previously made a bootloader that calls a main program in FLASH memory. Do I call a program in SRAM the same way?2011-05-17 4:20 AM
It's going to run quite a bit slower then when running in FLASH
2011-05-17 4:20 AM
Hi sima, obtronix,
Thanks for the comments, Note also to remap the interrupts into RAM if you them in your application. Running program from RAM is useful for user boot-loader applications or to program the Internal flash as well. Cheers, ST1.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.