2021-02-05 7:41 AM
Hi everyone,
I recently revamped a product with a STM32F427 with a new STM32H745.
Both cards have an external RAM of 16Mbyte. In the STM32F4 the data bus is 16bit width while in the SRM32H7 the data but is 32bit width.
Both cards are set to go to the maximum speed @168MHz for the STM32F4 to 480MHz for the STM32H7.
I noticed that with simple memory access operations such as (memcpy, arm_copy_q31, memset and arm_fill_q31) I obtained very different values and that do not return with the performance that I would have expected. (see attached file). In particular it seems that STM32F4 is faster than the other STM32H7 despite having a much lower clock.
Also I don't explain why, the operations performed on SRAM_D1 and DTC_RAM have comparable execution times even if on DTC_RAM should be much faster.
Here is a few code used to check performance:
startTimeTest=HAL_GetTime_us();
memcpy(DestIntTest,SourceIntTest,50000*sizeof(uint8_t));
Timetest1=HAL_GetTime_us()-startTimeTest;
startTimeTest=HAL_GetTime_us();
arm_copy_q31((q31_t *)SourceIntTest, (q31_t *)DestIntTest, 12500);
Timetest2=HAL_GetTime_us()-startTimeTest;
startTimeTest=HAL_GetTime_us();
memcpy(DestExtTest,SourceExtTest,1000000*sizeof(uint8_t));
Timetest3=HAL_GetTime_us()-startTimeTest;
startTimeTest=HAL_GetTime_us();
arm_copy_q31((q31_t *)SourceExtTest, (q31_t *)DestExtTest, 250000);
Timetest4=HAL_GetTime_us()-startTimeTest;And here the clock setup on STM32H7:
void SystemClock_Config_HSE(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 5;
RCC_OscInitStruct.PLL.PLLN = 192;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_2;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 4096;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
while(1) { ; }//>> Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV1;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
{
while(1) { ; }//>> Error_Handler();
}
/* HSI48 for USB Clock */
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USB;
PeriphClkInitStruct.UsbClockSelection = RCC_USBCLKSOURCE_HSI48;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
while(1) { ; }
}
/* Set the ADC peripheral clock*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_ADC;
PeriphClkInitStruct.PLL2.PLL2M = 1;
PeriphClkInitStruct.PLL2.PLL2N = 18;
PeriphClkInitStruct.PLL2.PLL2P = 1;
PeriphClkInitStruct.PLL2.PLL2Q = 2;
PeriphClkInitStruct.PLL2.PLL2R = 2;
PeriphClkInitStruct.PLL2.PLL2RGE = RCC_PLL2VCIRANGE_3;
PeriphClkInitStruct.PLL2.PLL2VCOSEL = RCC_PLL2VCOMEDIUM;
PeriphClkInitStruct.PLL2.PLL2FRACN = 6144;
PeriphClkInitStruct.AdcClockSelection = RCC_ADCCLKSOURCE_PLL2;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
while(1) { ; }
}
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SPI5|RCC_PERIPHCLK_SPI4;
PeriphClkInitStruct.Spi45ClockSelection = RCC_SPI45CLKSOURCE_D2PCLK1;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
while(1) { ; }
}
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_UART4;
PeriphClkInitStruct.Usart234578ClockSelection = RCC_USART234578CLKSOURCE_D2PCLK1;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
while(1) { ; }
}
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I2C4;
PeriphClkInitStruct.I2c4ClockSelection = RCC_I2C4CLKSOURCE_D3PCLK1;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
while(1) { ; }
}
/* Enable SYSCFG clock mondatory for I/O Compensation Cell */
__HAL_RCC_SYSCFG_CLK_ENABLE() ;
/* Enables the I/O Compensation Cell */
HAL_EnableCompensationCell();
/** Enables the Clock Security System
*/
HAL_RCC_EnableCSS();
}Any help will be appreciated.
thanks in advance,
DM
2021-02-05 7:48 AM
I do not see any cache setup here. Without the caches, CortexM7 will crawl...
2021-02-05 8:16 AM
Yes there is this at startup:
int main(void)
{
U32 zTimeout;
HalErr_tError zHalErr;
LibErr_tError zLibErr;
/* wait until CPU2 wakes up from stop mode */
zTimeout = 0xFFFF;
while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) == RESET) && (zTimeout-- > 0));
if ( zTimeout <= 0 )
{
while(1){};
}
/**/
HAL_Init();
/* Configure the system clock to 480 Mhz */
SystemClock_Config_HSE();
/* Enable the CPU Cache */
CPU_CACHE_Enable();
/* Configure the MPU attributes as Write Through for SDRAM */
MPU_Config();
....where CPU_CACHE_Enable:
static void CPU_CACHE_Enable(void)
{
/* Enable I-Cache */
SCB_EnableICache();
/* Enable D-Cache */
SCB_EnableDCache();
}and this:
static void MPU_Config(void)
{
/* MPU Configuration, to disable cache on frame buffer */
MPU_Region_InitTypeDef MPU_InitStruct;
/* Disables the MPU */
HAL_MPU_Disable();
/* Configure the MPU attributes for SDRAM */
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.BaseAddress = SDRAM_DEVICE_ADDR;
MPU_InitStruct.Size = MPU_REGION_SIZE_16MB;//>>MPU_REGION_SIZE_32MB;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.SubRegionDisable = 0x00;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Configure the MPU attributes for SRAM_D3 to normal memory not cacheable */
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER1;
MPU_InitStruct.BaseAddress = 0x38000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_64KB;
MPU_InitStruct.SubRegionDisable = 0x0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL1;//>>MPU_TEX_LEVEL1;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/** Initializes and configures the Region and the memory to be protected
*/
/* Ethernet description area */
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER2;
MPU_InitStruct.BaseAddress = 0x30040000;
MPU_InitStruct.Size = MPU_REGION_SIZE_256B;
MPU_InitStruct.SubRegionDisable = 0x0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/** Initializes and configures the Region and the memory to be protected
*/
/* Ethernet Heap area. See LWIP_RAM_HEAP_POINTER */
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER3;
MPU_InitStruct.BaseAddress = 0x30044000;
MPU_InitStruct.Size = MPU_REGION_SIZE_16KB;
MPU_InitStruct.SubRegionDisable = 0x0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL1;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Enables the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
}
2023-04-03 7:55 AM
Hi, Did you get to the bottom of your performance (ore lack of it) problem?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.