cancel
Showing results for 
Search instead for 
Did you mean: 

ST32Cube_FW_H7 V1.5.0 Nucleo H743Zi code for LED2 doesn't work.

Richard Li
Senior

I used ST32Cube_FW_H7 V1.5.0 Nucleo H743Zi example code for Nucleo H743Zi, the LED2 doesn't work, I thought I got bad module, then I order again, second Nucleo doesn't work too.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4

There are two different H743ZI boards, make sure you're building for the right one, check the command line define passed to the linker, and then at the #ifdef's in the include file with LED2 etc in it.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Richard Li
Senior

​Thank you, Clive1!

I only got one schematics, it doesn't match my board.

Do you know where I can find MB1137 Rev B schematics?

Richard

Richard Li
Senior

Thank you, Clive1!

This only for manual, it din't include schematics.

Richard

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.