2009-08-06 7:30 AM
ST32_USB-FS-Virtual com loop back test - FAIL ?
2011-05-17 4:19 AM
Gentleman,
I found some problems with accuracy of ST32 USB Virtual com implementation. I hope I am wrong , but I can not find the reasonable explanation of my problem. Plz, help me with this …. Initially, I had an practical tack to transfer data from preferential device , which I designing to PC for visualization. I must transfer 1000 packets of data (each packet is 50 bytes) at 38400 speed. Each packets is a set of characters ( line of text ) and I can easy verify the accuracy of data transmission just screen of any PC data terminal. For testing proposes all packets have the same data, therefore in case of success I must see 1000 identical lines of texts. I checked the data stream with a scope : I had approximately 15 mS of transmission time for each packet and 10 mS for a pause between the packets. The transmitter is also confirm with packets transmission with the CTS signal . In the beginning , I connected the transmitter of the packets to PC by “off the shelf�? Serial_to_USB cable (Prolific) and check the accuracy of transmitted data on the screen of data terminal( “bray_terminal�? ). In this configuration of hardware , I had no problem at all – I can see on my screen 1000 lines of identical text : --------8<---------------------- !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6B !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6B !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6B !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6B !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6B !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6B !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6B !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6B !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6B !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6B !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6B --------8<---------------------- After this I decided to transfer the same data to PC terminal by regular USB cable , but over ST32 Virtual Com Port. I programed the Olimex H103 board with the latest ST Virtual Com Port firmware. I got the source code from UM0424 and compiled it with IAR 5.30. Olimex ST32-H103 board is not matching the source hardware exactly and I did small modification in source code : /* #define USB_DISCONNECT GPIOD #define USB_DISCONNECT_PIN GPIO_Pin_9 #define RCC_APB2Periph_GPIO_DISCONNECT RCC_APB2Periph_GPIOD */ #define USB_DISCONNECT GPIOC #define USB_DISCONNECT_PIN GPIO_Pin_11 #define RCC_APB2Periph_GPIO_DISCONNECT RCC_APB2Periph_GPIOC After this I programed the H103 flash and added 7 centimeters ( it is around 3 inches ) jumper wire from output of RS232 transmitter ( 3,3 V ) to input RX pin of UART1 on ST32-H103 board ( pin 7 , header 1 ) . For sure the fat wire for ground was connected too. Suggested Virtual COM port driver for Vista was installed . Same terminal software again. This is my result trough ST32 virtual com port : --------8<---------------------- !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6B !A555,1,1,,A,fOoNLrK8`KMOwQfFAliCPMnA0U,0*6B !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6B !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6B !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6B !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6B !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliP:MnA0U,0*6B !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6B !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6 !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6B !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6B !AI555,1,1,,A,fOoNLrKM8`KMOwQfFAliCP:MnA0U,0*6B --------8<---------------------- Us you can see some characters is missing . Approximately 30 % of packets is garbage – this result is not adaptable. Initially I was under impression that a have a problem with hardware. I did a double check and did not find any trouble. Finally, I decided to run a loop back test for both hardware configuration. I found in the Internet the loop back test with was created by Luciano: http://www.mcselec.com/index.php?option=com_content&task=view&id=165&Itemid=57 I tested the Prolific cable with loop back jumper and this cable pass the test at any com speed. After this I placed short jumper between pin 4 and pin 7 of header at ST32H103 board and ran the same test again for ST32H103 board . Unfortunately , the test fail at any com speed. Is somebody have the reasonable explanation of this results ? Can somebody repeat the test on different hardware ? ( you must place just a single jumper wire ) Thanks for you cooperation. Alex.2011-05-17 4:19 AM
Problem solved.
In the attached file the source code from Olimex web site with was adapted for H103 board. Now it is working and pass the feedback test. I Hope it will help to somebody. Regards, AlexWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.