2018-05-28 11:11 PM
I need to program external memory using CLI. Conventional programming using the software is succesfull. Need to integrate the commands for the labview programming.
C:\Project\Programming\ST-LINK Utility>ST-LINK_CLI.exe -P assets.hex -EL MX25L512G_STM32F769I-DISCO.stldr
STM32 ST-LINK CLI v3.0.0.0STM32 ST-LINK Command Line InterfaceST-LINK SN : 48FF6C067266535216230367
ST-LINK Firmware version : V2J29S7Connected via SWD.SWD Frequency = 4000K.Target voltage = 3.1 V.Connection mode : Normal.Device ID:0x451Device flash Size : 2048 KbytesDevice family :STM32F76xLoading file...Flash Programming: File : assets.hex Address : 0x90000000 External Loader File : MX25L512G_STM32F769I-DISCO.stldr Device Name : MX25L512G_STM32F769I-DISCO Device Start Address : 0x90000000 Device Size : 0x04000000 Device Type : Nor FlashMemory programming...¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦ 0%Timeout during flash programmingError occured during erase operation!Programming Complete.is the any additional parameter need to be type into it? I have tried with the latest version seem not succesfullly done both using the GUI or CLI
2018-05-29 2:33 AM
Hello
izal.muin
,I recommend you to use the new
software tool delivers device-programming and firmware upgrade for STM32 microcontrollers.
Best Regards
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.