2015-07-06 9:03 AM
Hi, I am new to working with the ST LINK.
I downloaded the ST-LINK/V2 firmware upgrade from the site. When attempting to run the jar file I got an error: ''Architecture not supported(arm)'' Could someone please help2015-07-06 11:16 AM
Assume we know nothing about your system, or the specific file you downloaded.
2015-07-08 4:33 AM
I am running the raspberry pi b+ v1.2
The file I downloaded was: Part Number - STSW-LINK005, Version - 2.24.4,2015-07-08 5:49 AM
The error suggests it's expecting an x86 based system.
2015-07-08 7:41 AM
Yes, I thought as much.
I have trace the problem to a driver(libSTLinkUSBDriver.so) that was compiled for x86 and x64. Is there however any way to get it to work with arm2015-07-08 10:43 AM
Is there however any way to get it to work with arm
I doubt there's a strong commercial driver, your use case is a bit of an outlier. Perhaps they are using GPL code requiring the release of source?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.