2016-01-23 4:04 AM
I am using ST-Link V2 to flash to STM32F747, It was successful. However, after sometimes change the code IAR pop-up below warnings:
Warning: Write failed (CPU data abort) at Memory address 0x2001EF98Warning: Write failed (CPU data abort) at Memory address 0x2001EF84
Failed to set breakpoint at 0x200000C4 (out of breakpoints?)
After that I could not flash the MCU anymore.
Do you know how to troubleshoot this issue?Thank You!2016-01-23 10:04 AM
Do you know how to troubleshoot this issue?
Hard to say, not really overwhelmed with detail here.What exactly did you change in the code between the time it was functioning normally, and the time it started misbehaving?Is this a board you designed yourself, or something else? The clocks and power supplies would be a good place to start.If this is an external ST-LINK, make sure you have current firmware, and try accessing the device with the ST-LINK Utilities.2016-02-22 2:02 AM
I changed a lot in code and could not trace which part has the issue. I have coded again from the point sw working.I used another board and flash with another code, then it works. The board is designed by myself.
It seems the MCU is dead but I still don't know it is caused by SW or HW. I stored the hex file when MCU died. But I am scare to test. The MCU is STM32F746IGT6 ________________ Attachments : STM32746IG_Mic_Array.hex : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0x5&d=%2Fa%2F0X0000000bg6%2FliNitW9rxTzGk2vSXZwmV0XQy8NfXGAIskM_x04PCUE&asPdf=false2016-02-22 12:51 PM
I know nothing about your board, so the .HEX file really isn't going to help me much.
You should perhaps put your problem chip into the System Loader (BOOTx pins), and see if you can communicate with that via a USART, or if you can get it to come up in DFU mode via the USB connection if your board has one.Your should be able erase the chip with the ST-LINK Utilities while it executes the System Loader rather than your code.2016-02-22 9:34 PM
The last error message suggests you have too many breakpoints set. You're limited to a certain number by hardware. If you try to debug a session, it'll fail. It should still flash though, at least it does with Eclipse.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.