2016-08-22 5:52 AM
Hi All,
Connect the pins were as follows: SWD ST-LINK V2 and between MCU.1:VDD - VDD3:GND - GND7:SWDIO - PA13_SWDIO 9:SWCLK - PA14_SWCLKPDR_ON: 10k pull-upBOOT0: 10k pull-downBYPASS_REG: 10k pull-downVCAP: 2.2uF GNDVDD:1.8VVDDUSB:1.8VVBAT:1.8VVDDA:1.8VThe test MCU is in STM32F746NGH6.VDD is 3.3V when the connection was good, do not connect change with VDD 1.8V, as shown below.On the MCU specifications are listed as available from 1.7V to 3.6V.Can not connect to target!Please select ''Connect Under Reset'' mode from Target->Settings menu and try again.If you're trying to connect to a low frequency application , please select a lower SWD Frequency mode from Target->Settings menu.What's the problem?Thank you.
Best regards,gyosun.
2016-08-22 6:22 AM
Hi gyosun,
Upgrade the ST-Link firmware to V2-1 version through this and try again. -Hannibal-2016-08-22 7:38 AM
VDDUSB isn't going to be viable at 1.8V
I seem to have to constantly repeat the same advice. Review the voltage on the VCAP and NRST pins. Connect NRST on the debugger header. Consider if the ST-LINK is supporting 1.8V through it's buffers. Not really going to dig into the PDR/BYPASS Consider if you can connect to the USART in the System Loader (BOOT0=1) to see if you can show signs of life for the STM32 chip that way.2019-02-02 5:23 AM
I have same problem with battery powered custom board with STM32L431. The MCU connects successfully when VDD is under 3.3V but not above 3.3 - 3.6V. The configuration as follow
VDD is about 3.6V
GND
NRST
SWDIO -> PA13
SWDCLK -> PA14
SWO -> PB3
Any suggestion? Thanks in advance.
ierturk
2019-02-02 5:32 AM
And this is using an official ST-LINK/V2 or some bootleg?
2019-02-02 5:37 AM
Yes it is official ST-LINK/V2.
2019-02-02 5:40 AM
Yes it is official ST-LINK/V2.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.