2015-06-19 10:15 AM
Hi All
Using ST-Link 3.6.0 to download a HEX file to an STM32F407 board I found that the loaded code sometimes didn't run. But, if I loaded the BIN version instead it was OK. After some investigation I found that the HEX file sometimes had lines like this: :10AAC0004100546F3A20000D0A5375626A65637441 :10AAD0003A20000D0A46726F6D3A20000D0A2E00D2 :0FAAE00005060C181C3C082008001100015180CD <---- :10AAF000746573745F6E616D6540746573742E6305 :10AB00006F6D000000000000000000000000000069 :10AB1000000000000000000000FFC29EE50B0000E6 Notice that most lines are 0x10 bytes in length but one is 0x0f. There is in fact a single byte ''hole'' in the object. After loading with ST-Link and successful verification the code would not run. Debugging the case it was found that the line :10AAF000746573745F6E616D6540746573742E6305 is not programmed in Flash to 0xaaf0 as expected but is programmed to 0xaaef - where the 'hole' should be. The result is that the program content after this line is shifted by one byte. In the investigated case the content was const values but when the program accessed them they were one-off and in the case of critical values it would lead to the code failing. As I wrote - if I load the BIN instead of the HEX the code is correct in Flash. Aslo, I don't always get the 'hole' in the code (it is due to consts being aligned to a long word boundary) and then all works too. Is this a known issue with the tool?? Regards Mark #st-link-hex-bug2015-06-19 11:38 AM
Is this a known issue with the tool??
I've seen it reported here before, might dig for a cite. Seem to be several broken tools on the site for quite some time. This is one of those insidious problems one would have hoped was addressed promptly.2015-06-19 11:56 AM
Here's the one I remembered
I'm going to push this up to moderation.2015-06-20 5:36 AM
Hello Clive
Thank you very much - I did a search to see whether it was a known issue but didn't hit the post that you linked to. However it is indeedexactly the problem
. In fact it is a very serious issue in such a tool since it is obviously not using the HEX addressing correctly and just seems to be linearly writing to Flash. Hope it will be corrected to avoid others losing time debugging the same issue which turns out to be a tool error rather than a SW error! Regards Mark2015-06-25 10:32 AM
This is very interesting as I have used the command line version to program tens of thousands of STM32Fxxx parts without seeing this issue.
I wonder if it is specific to the environment the GUI utility is running in? (I do use the GUI utility, but only a few hundred cycles per year.) In the last five years, I've never had a HEX file fail to load for this issue.2015-06-25 10:52 AM
Probably depends more on the tools generating the .HEX, and if it creates voids.
ST hasn't responded to anyone, and I'm not going to do regression testing on it, to understand when it was broken, or if it ever worked.This is generally why I write my own programming software, as blaming someone else doesn't put out fires on the production floor.2015-07-30 2:06 PM
I don’t know where to report this but I tried ST-Link V3.6 to load hex file, it didn’t work and I downgrade it to V3.5, it is working. It seems like the problem with v3.6 is when it reads hex files, some of the bytes shifted by one to the left.
Regards
2015-07-30 4:52 PM
Have you tried v3.7?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.