2018-08-23 9:29 AM
Hi,
I am seeing the issue since yesterday for unable connect to target. Here is the message from TrueSTUDIO. Unable to connect using STM32 ST-LINK Utility as well.
I am guessing the ST-LINK device burned. We are using tag-connect TC2050 adapter and connector. My question is what might burn ST-LINK? How to know if the ST-LINK device is mal-function?
Thx
http://www.tag-connect.com/Materials/TC2050-ARM2010.pdf
Atollic TrueSTUDIO gdbserver for ST-Link. Version 4.2.2 (WIN32 2018-02-26 16:20:21 15675)
Copyright (c) 2018, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistant Mode : Disabled
LogFile Name : debug_log.txt
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Target unknown error 5010512
Error in initializing ST-Link device.
Reason: Unknown. Please check power and cabling to target.
2018-08-23 11:07 AM
>>How to know if the ST-LINK device is mal-function?
Test it on a working target? Have two so you can compare/contrast?
>>My question is what might burn ST-LINK?
The buffers, regulators or STM32F1
2018-08-23 11:35 AM
Found it, the VAPP (target VCC) on the JTAGE 20-pin connector is not right. Issue is on our board. Thx
2018-08-24 6:49 AM
Hi @Dick Lin ,
Thanks a lot for sharing the solution. For sure, this will be helpful for other users facing the same issue.
Khouloud.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.