2019-07-18 6:06 AM
Hardware tested and functional.Commands modified on QSPI example (STM32Cube_FW-F7_V1.15.0) and the erase, read and write commands are functional.Problem to develop an externa loader, based on STM32F769I-EVAL example(using SW4 and MDK-ARM).The MDK_ARM example has scatter file errors (segment order) and the external loader not recognize the file.I need information how to develop the external loader.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.