2014-01-19 10:48 AM
hello every one , i tried to show picture on 3.2'' tft lcd that use SSD1289 driver,
i can fill , write char and ... correctlybut i cant show picture , many pixels writes wrong and this wrong changes with reset of board! this problem Cause the picture that shown , cant be Recognizablethanksalireza roozitalab2014-01-21 12:40 AM
i use fsmc and i have your problem i can fill color and display text char but picture not display correct .and my lcd hang in any time and many times my lcd is failed to start up or stop work ??
the problem is gpio and fsmc time are faster than lcd module ssd1289 try to low it's speed try this this work not good's alot but work GPIO_InitTypeDef GPIO_InitStructure; RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD | RCC_AHB1Periph_GPIOE, ENABLE); GPIO_PinAFConfig(GPIOD, GPIO_PinSource0, GPIO_AF_FSMC); // D2 GPIO_PinAFConfig(GPIOD, GPIO_PinSource1, GPIO_AF_FSMC); // D3 GPIO_PinAFConfig(GPIOD, GPIO_PinSource4, GPIO_AF_FSMC); // NOE -> RD GPIO_PinAFConfig(GPIOD, GPIO_PinSource5, GPIO_AF_FSMC); // NWE -> WR GPIO_PinAFConfig(GPIOD, GPIO_PinSource7, GPIO_AF_FSMC); // NE1 -> CS GPIO_PinAFConfig(GPIOD, GPIO_PinSource8, GPIO_AF_FSMC); // D13 GPIO_PinAFConfig(GPIOD, GPIO_PinSource9, GPIO_AF_FSMC); // D14 GPIO_PinAFConfig(GPIOD, GPIO_PinSource10, GPIO_AF_FSMC); // D15 GPIO_PinAFConfig(GPIOD, GPIO_PinSource11, GPIO_AF_FSMC); // A16 -> RS GPIO_PinAFConfig(GPIOD, GPIO_PinSource14, GPIO_AF_FSMC); // D0 GPIO_PinAFConfig(GPIOD, GPIO_PinSource15, GPIO_AF_FSMC); // D1 GPIO_PinAFConfig(GPIOE, GPIO_PinSource7, GPIO_AF_FSMC); // D4 GPIO_PinAFConfig(GPIOE, GPIO_PinSource8, GPIO_AF_FSMC); // D5 GPIO_PinAFConfig(GPIOE, GPIO_PinSource9, GPIO_AF_FSMC); // D6 GPIO_PinAFConfig(GPIOE, GPIO_PinSource10, GPIO_AF_FSMC); // D7 GPIO_PinAFConfig(GPIOE, GPIO_PinSource11, GPIO_AF_FSMC); // D8 GPIO_PinAFConfig(GPIOE, GPIO_PinSource12, GPIO_AF_FSMC); // D9 GPIO_PinAFConfig(GPIOE, GPIO_PinSource13, GPIO_AF_FSMC); // D10 GPIO_PinAFConfig(GPIOE, GPIO_PinSource14, GPIO_AF_FSMC); // D11 GPIO_PinAFConfig(GPIOE, GPIO_PinSource15, GPIO_AF_FSMC); // D12 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_7 | GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_14 | GPIO_Pin_15; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; //NOPULL UP GPIO_Init(GPIOD, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7 | GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; //NOPULL UP GPIO_Init(GPIOE, &GPIO_InitStructure);2014-01-24 11:35 AM
2014-01-25 1:48 PM
test code at low cpu frequency like 42MHz .
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.