2024-03-08 1:01 PM
I'm trying to send ADC results over to a receiver via UART, but somewhy the program freezes on sprintf() IF I have called HAL_ADC_Start_DMA() before. If I call sprintf() before HAL_ADC_Start_DMA() it works fine. However, I need to call it after starting the DMA. How can I fix this?
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* Configure the peripherals common clocks */
PeriphCommonClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_MEMORYMAP_Init();
MX_ADC1_Init();
MX_LPUART1_UART_Init();
/* USER CODE BEGIN 2 */
uint32_t values[4] = {0, 0, 0, 0};
HAL_ADC_Start_DMA(&hadc1, values, 4);
char str[100];
sprintf(str, "TEMP_ADC: %d\n", values[1]);
int size = (int)(ceil(log10(values[1]))+12)*sizeof(char);
HAL_UART_Transmit(&hlpuart1, str, size, 100);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_8, SET);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
HAL_Delay(1000);
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
2024-03-08 3:15 PM
>>Do I also need to change the 'Number of Conversions' in the .ioc?
I don't know, I just code for myself.
Fix whatever you need to associate the size of the buffer, with the DMA, assuming the 4's here, but would assume the ADC is only 16-bit wide.
uint32_t values[4] = {0, 0, 0, 0};
HAL_ADC_Start_DMA(&hadc1, values, 4);One of the problems is that if sampling fast enough you'll end up with interrupts at 500 KHz to 1 MHz, which will be too hard for the processor do much else than enter/exit the interrupt handler. And none of your foreground code will have any time to execute.
You could try decimating the "sample rate" such that it might run at a few KHz
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.