2021-03-20 7:57 AM
I have a Pi that sends data to the MCU via SPI. I have the SPI running in DMA circular buffer mode on the MCU. In the TxRx callback, the data from the Pi is processed, and then the motors are turned ON/OFF, etc.
This works, however, each time the Pi sends data to the MCU, any motors that are already running and are meant to continue running, pause for just a moment and then continue running. Why does this happen and more importantly how do I ensure the motors run continuously without pause?
I know that the callbacks are supposed to be really light on code, but I see the same behavior when I remove the motor control function inside the infinite while loop in main.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.