2018-08-31 6:31 AM
I'm trying to communicate between the nucleoh743 (master mode) and a TDC GP22 slave chip but came across this issue:
I am expecting to read 0x27 but i always get 0x26. All the other bits from this 1 byte are correct so i was wondering if there something else that is wrong other than the slave device. Here is a pic from the logic analyzer. (CPOL=0, CPHA=1). The SPI init code was produced by cubemx.
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET); // CS
HAL_Delay(1);
HAL_SPI_Transmit(&hspi1, &tx, 1, 1); // transmit 0xB5 from uint8_t tx
HAL_Delay(1);
HAL_SPI_Receive(&hspi1, &rx, 1, 1); // store in uint8_t rx
HAL_Delay(1);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_SET); // CS/* SPI1 init function */
static void MX_SPI1_Init(void)
{
/* SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_128;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 7;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
hspi1.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
hspi1.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
hspi1.Init.TxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
hspi1.Init.RxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
hspi1.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
hspi1.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
hspi1.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
hspi1.Init.IOSwap = SPI_IO_SWAP_DISABLE;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}thanks
2018-09-06 10:32 AM
For what is worth, i changed the microcontroller to a stm32f4 and there are no more problems with the LA...
2018-11-11 10:58 PM
Hi, i write a test code for gp22 , generated hal cube mx for stm32f107vctx..and my problem is a miso pin,miso pin is 0 ..i confused beacuse i connect a led to intn pin of gp22 and when send 0x03 for cal resonator its worked and give me a innterupt ...but miso any thing send...
please help me.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.