2019-07-21 6:28 AM
I have a problem with setting up SPI1 in Master mode using the following code. I set the SSM bit to enable software slave management, but when I try to enable the SPI by setting the SPE bit, the MSTR bit is cleared.
Thanks for help.
Jaroslav
RCC->APB2ENR |= RCC_APB2ENR_IOPAEN | RCC_APB2ENR_AFIOEN | RCC_APB2ENR_SPI1EN;
GPIOA -> CRL &= 0x000FFFFF;
GPIOA -> CRL |= 0xB4B00000; /// PA7 - MOSI, PA6 - MISO, PA5 - SCK
SPI1->CR1 &= ~SPI_CR1_BR; // baud rate = fpCLK/2
SPI1->CR1 &= ~SPI_CR1_CPOL;
SPI1->CR1 |= SPI_CR1_CPHA;
SPI1->CR1 &= ~SPI_CR1_DFF;
SPI1->CR1 &= ~SPI_CR1_LSBFIRST;
SPI1->CR1 |= SPI_CR1_SSM; // software slave management
SPI1->CR1 |= SPI_CR1_MSTR;
SPI1->CR1 |= SPI_CR1_SPE;
2019-07-21 4:12 PM
Which STM32?
When you set SSM, the SS input is governed by state of SSI bit - if it's 0, it's the same as if you'd not set SSM and pulled the NSS pin low, i.e. it switches to slave mode.
JW
PS. A stylistic one: I prefer to set peripheral registers all at once, in a single write, instead of a series of RMW operations.
2019-07-31 9:12 AM
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.