2018-07-13 9:36 AM
Hi,
I am working on Nucleo-144 SPI. The NSS GPIO ios PA4. The only way I can have the NSS high is use
__HAL_SPI_DISABLE() function. The HAL_GPIO_WritePin() just never work.
I can see from the scope to verify it. Doesn't seems to be the right way to turn off the SPI for set NSS high.
Anyone has experience turn NSS high/low?
/**SPI1 GPIO Configuration
PA4 ------> SPI1_NSS PA5 ------> SPI1_SCK PA6 ------> SPI1_MISO PA7 ------> SPI1_MOSI */HAL_GPIO_WritePin( GPIOA, GPIO_PIN_4, GPIO_PIN_SET ); // NSS1 high
__HAL_SPI_DISABLE(m_spi);
Thx
2018-07-15 9:28 PM
Hi,
I just saw this example. Need to leave the PA4 pin to be a generic GPIO pin.
Thx
https://visualgdb.com/tutorials/arm/stm32/spi/
We will leave the PA4 pin to be a generic GPIO pin to demonstrate how to
control the NSS signal manually:
GPIO_InitStruct.Pin = GPIO_PIN_4;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
On Sun, Jul 15, 2018 at 7:08 PM, Clive Two.Zero <
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.