2012-09-13 2:40 PM
I'm tring to set up SPI2 as a master SPI device to communicate with another device. After configuring the clocks, GPIO and SPI device, I wait for SPI_I2S_FLAG_TXE to clear before writing. But the flag never clears, so I'm stuck. I took this code as close as possible from the examples included with the peripheral library. I'm not sure if I'm missing any other setup steps.
static void InitSPI( void )
{ GPIO_InitTypeDef GPIO_InitStructure; SPI_InitTypeDef SPI_InitStructure; // PCLK2 = HCLK / 2 RCC_PCLK2Config(RCC_HCLK_Div2); // Enable GPIO clock for SPI2 RCC_APB2PeriphClockCmd( RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB | RCC_APB2Periph_AFIO, ENABLE); RCC_APB1PeriphClockCmd( RCC_APB1Periph_SPI2, ENABLE );//
//Allocate GPIO pins to SPI interface ////Initialize GPIO config struct
GPIO_StructInit(&GPIO_InitStructure); //Pins B13 and B15 GPIO_InitStructure.GPIO_Pin = ( GPIO_Pin_13 | GPIO_Pin_15 ); GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOB, &GPIO_InitStructure);//Pins B14
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_14; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOB, &GPIO_InitStructure);// //Configure SPI bus // //Initialize SPI config struct SPI_StructInit(&SPI_InitStructure);
//Set SPI config struct
SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low; // idle logic low SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; // capture on falling edge SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_8; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_Init(SPI2, &SPI_InitStructure);// Enable SPI_MASTER NSS output for master mode
SPI_SSOutputCmd(SPI2, ENABLE); // Enable SPI_MASTER SPI_Cmd(SPI2, ENABLE); } The problem occurs just before the read: //Wait for SPI2 Tx buffer empty while (SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_TXE) == RESET); //Send first byte to start read SPI2->DR = SPI_CMD_READ; #stm32-spi2012-09-13 3:49 PM
TXE goes high when the holding buffer is empty.
When initially writing DR, expect it to go low briefly, then high again as the first byte moves from the holding register to the shift register, subsequent bytes will see it remain low for longer, typically 8 or 16 bit times depending on the settings.2012-09-14 1:11 AM
Clive,
Geoff is apparently aware of the ''inverse'' nature of the TXE bit (although the ''wait for clear'' wording is misleading indeed):> //Wait for SPI2 Tx buffer empty
> while (SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_TXE) == RESET); Geoff, Did you switch on the APB1 clock? JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.