2018-07-01 1:57 AM
I have strange problem, SPI is sending 16 clocks instead of 8 as configured, and my trinamic motor driver simply does not work. Same code worked for STM32F415, right now i am using STM32F051
GPIO_InitTypeDef GPIO_InitStructure;
SPI_InitTypeDef SPI_InitStructure; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5|GPIO_Pin_6|GPIO_Pin_7; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_0); GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_0); GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_0); SPI_I2S_DeInit(SPI1); SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; // define for it is ((uint16_t)0x0700) SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low; SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_32; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_Init(SPI1, &SPI_InitStructure); SPI_Cmd(SPI1, ENABLE);It looks like normal code, so i don't know what to do now. If i set to 4 bits, it works (generates 8 clocks) , if i set to 8b i always get 16 clocks.
Is it some kind error in silicon? or in SPL libraries ?
Sending is done like this:
while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE));
SPI1->DR=(uint8_t)address;while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE));R=SPI1->DR;2018-07-01 4:59 PM
>>Is it some kind error in silicon? or in SPL libraries ?
NO
The newer families of STM32 have a FIFO on the SPI, and queue a 16-bit write as a pair of 8-bit byte
while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE));
*((volatile uint8_t *)&SPI1->DR) = (uint8_t)address; // Do a 8-bit wide write at the peripheral bus
while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE));
R=*((volatile uint8_t *)&SPI1->DR);2018-07-06 4:26 AM
I see now, it is more complicated.
digging to libraries i found different sending function: (Flag check is not included in send function)while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE));
*(__IO uint8_t *) ((uint32_t)SPI1+0x0C) = data; while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE)); return *(__IO uint8_t *) ((uint32_t)SPI1+0x0C);it always hangs on while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE));
But if i comment it, i will get one cycle delay in my SPI register.in other words, if i short MISO and MOSI, send 0xAA, i will get back 0, and second time, i will get 0xAA, so it i useless for my implementation.
How can i get clock in data with no latency ?
2018-07-06 5:10 AM
it always hangs on while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE));
Should not.
If you observe the SPI registers using debugger, stop doing that.
JW
2018-07-06 5:14 AM
I only observe global variables in real time so i know whats going on. i don't use debugger to see direct registers, only stepping code with debugger, that's all
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.