2012-08-17 3:19 PM
I am trying to receive data over full duplex SPI but STM32 does not line up clock and data if I configure in SPI_CPHA_2Edge. However if I configure in SPI_CPHA_1Edge, everything works fine. My slave however sends data in 2Edge. Does anybody have a workaround on this?
void configure_spi(void){ //Init GPIO structure GPIO_InitTypeDef GPIO_InitStructure; //Init SPI structure SPI_InitTypeDef SPI_InitStructure; //Enable SPI clocks RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1,ENABLE); RCC_PCLK2Config(RCC_HCLK_Div1); //DEFAULT WAS Div2 /* Enable GPIO clocks */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); //Set GPIOs GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; //GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7; //GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4; //SS GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5; //CLK GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; //MISO GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; //MOSI GPIO_Init(GPIOA, &GPIO_InitStructure); /* Connect SPI pins to AF5 */ GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_SPI1); //CLK GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_SPI1); //MOSI GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_SPI1); //MISO SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low; SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Hard; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; //SPI_BaudRatePrescaler_8 = 6.7MHz //SPI_BaudRatePrescaler_4 = 13.xMHz //SPI_BaudRatePrescaler_2 = 26.8MHz SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_8; //SPI1- for CLK, DATA, CS(DIR) SPI_Init(SPI1,&SPI_InitStructure); //SPI_TIModeCmd(SPI1, ENABLE); //SPI_I2S_ITConfig(SPI1, SPI_I2S_IT_RXNE, ENABLE); SPI_SSOutputCmd(SPI1,ENABLE); SPI_Cmd(SPI1,ENABLE); }uint8_t mip_Send_Receive_Byte(uint8_t byte){ /*!< Loop while DR register in not emplty */ while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET); /*!< Send byte through the SPI1 peripheral */ SPI_I2S_SendData(SPI1, byte); /*!< Wait to receive a byte */ while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET); /*!< Return the byte read from the SPI bus */ return SPI_I2S_ReceiveData(SPI1);}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.