2009-02-21 12:53 AM
SPI config question
2011-05-17 4:03 AM
I am using the SPI1 peripheral on a STM32F103VE device to get A/D conversion values from a 16 bit AD7685 A/D converter. I have the following connections.
A/D ST-SPI SCK SPI1_SCK SDO SPI_MISO CNV SPI1_NSS I had specific questions on how to configure SP1_NSS port. The ST example which uses NSS does not actually configure the GPIO A port pin 4 for NSS. It just configures the SPI_NSS as: SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; I have just one slave, the A/D, so do I configure the NSS pin as Hardware or Software driven. Also since I am only using the SPI to read values from the A/D should i configure the direction of SPI for 1Line Rx? This is what I currently have for the configuration of SPI, I am not getting any data from the A/D so I am thinking that it might have something to do with the N_SS pin. SPI_InitStructure.SPI_Direction = SPI_Direction_1Line_Rx; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_16b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low; SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_4; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_LSB; //SPI_InitStructure.SPI_CRCPolynomial = 7; Any responses are greatly appreciated.2011-05-17 4:03 AM
Hi siddj;
I don't know if the slave-select pin of AD7685 is called CNV, if it is the case, I think that it has to be connected to GND and not to SPI1_NSS, because your A/D is a slave. B.R. M3allem.2011-05-17 4:03 AM
Hi, the pin is called, CNV. Earlier it was called CS and now it has more functions so its called CNV but it still would function as a CS.
What do i do with the NSS pin? Hardware/Software? Here is the data sheet for AD7685http://www.analog.com/static/imported-files/data_sheets/AD7685.pdf
Thanks.2011-05-17 4:03 AM
Good that you provided the data-sheet - I downloaded it myself to assist earlier.
STM32's SPI is not conventional as regards NSS_CS output. (you can read several large posts dealing with this, here) To keep things simple - here's my suggestion: 1) Analog data into your 16 bit ADC is sampled on the ''rising edge'' of CNV. You ''cannot'' achieve this with ''normal'' STM32 SPI set-up! 2) Tie the ADC chip's SDI pin to Vdd. On the rising edge of CNV (which you provide by a ''non-SPI'' GPIO) the state of SDI is latched - and you enter what is called by A-D ''CS mode.'' 3) Keep CNV high for the period tCONV (0.7 - 3.2 uS). After this - drop CNV signal (to low). 4) Now you generate 16 rising clock edges - A-D states that data is valid on ''either'' edge - falling edge gives fastest conversion results. (this from Fig. 35) Looks like a nice, fast, hi-res chip. I see no real advantage - in fact I see many ''gotchas/complications'' if you try to interface using STM32's SPI. Strongly suggest that you simply ''bit-bang'' - 2 GPIO outputs (CNV & CLK) and 1 GPIO input (SDO). Let us know how this works, please...2011-05-17 4:03 AM
Thank you for such an elaborate response.
My board has already been done so I am just working on getting the ADC to talk to my processor. 1. The VIO pin of the ADC is tied to VDD(3.3V). 2. CNV is tied to SP1_NSS. 3. SDO-MISO and SCK-SP1_SCK. Since it can send date on either edge i am guessing the CPOL and CPHA configuration does not matter. I have the data size setup to 16 bit and the direction of the SPI transfer is set to be ''SPI_Direction_1Line_Rx'' since I an only receiving data in the master mode. So I am only unsure about the NSS setting. If the NSS pin is driven low, the A/D should start the conversion and send out data. So how should i configure NSS? as hardware or software driven? Also do i need to configure the GPIO pins connected to SP1_NSS(pin A4). I have tried both ways and did not have much luck, still 0's in my data register. LEt me know if there is anything fundamentally wrong in my SPI config. I really appreciate your help, thanks!2011-05-17 4:03 AM
*
1. THE VIO and SDI pin of the ADC is tied to Vdd...sorry2011-05-17 4:03 AM
Don't hate me - as stated previously your attempt to ''master'' STM32's ''arcane'' SPI set-up/operation is delaying & complicating your stated task.
Again - look carefully @ A-D Fig 35. (I have my staff post such diagrams @ their workstation) This drawing shows that the analog conversion ''starts'' upon the rising edge of CNV. CNV should remain high for the conversion period (tCONV) and then is brought low. *** you can not achieve this effect using STM32's SPI operation - imho it is wasteful to even try! *** So - change your pin configuration from SPI to ''GPIO push-pull'' for CNV and A-D clk, change to ''GPIO input'' for A-D data output. This should enable you to ''keep'' your pcb routings intact. After period tCONV expires you bring CNV low - now you clock the A-D and I bet you data will start marching out of the A-D - and into your STM32. Hooking a scope or data analyzer to the A-D data out will comfort/assist. Only ''after'' you have this working with ''bit-bang'' would I revisit the SPI mode/operation. (but who cares - why bother?)...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.